cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G491CEU6 PA12 Getting Pulled Up during Bootloader

BGheb.1
Associate II

I'm currently trying to program the MCU using UART by entering bootloader using BOOT0 and nRST. However, whenever I send an nRST pulse PA12 gets pulled up and I'm not able to connect to the MCU. If I power cycle the board while BOOT0 is pulled high I can connect.

Adding a 50k pull-down resistor on PA12 allows me to connect successfully but I see 0.7V at PA12 after resetting.

I can't understand how I'm getting this voltage.

0693W00000GYe3bQAD.jpg

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

PA12 is the DP line for USB. The bootloader connects the internal pullup on this line to tell the host a USB device is present and listen for a signal.

If you have USB connected, the USB DFU bootloader will launch and prevent any other bootloader interfaces from being used. The first peripheral it sees will be the one it selects.

If you feel a post has answered your question, please click "Accept as Solution".