cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G431C8T6 SPI bootloader whole-chip CRC cmd was acknowledged but address after that received neither ACK or NACK

pxia.1
Associate II

my host interaction with STM32G431C8T6 SPI bootloader are functioning for a lot of jobs such as RW, but not for the whole-chip CRC. Here is the Logic analyzer captured data:

Host=>BL, BL=>Host

5A, A5

A1,A5

5E,A5 cmd to run whole chip CRC

00,A5

......

00,A5

00,79 BL confirms the cmd

no difference with or without 1sec delay here

08,A5 send 4 byte addr and chksum

00,A5

00,A5

00,A5

08,A5

00,A5 for ever, precisely speak, host keeps polling for 5 secs, and didn't even receive NACK

I follow AN4286 to design the host code. After going through STM knowledge base and existing furum threads, I hope someone could share some guidance with me. Thanks a lot.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0