STM32G4 USB-PD board restarting after SRC cababilities are recieved
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-10 7:00 AM
Hi!
I am having big troubles getting USB-PD sink on the STM32G431KBT to work. I am using CubeMX and following the AN5418 Complete USB-PD application example and using FREERTOS 10.3.1 and USBPD 3.3.0.
Connected to my wall adapter the debug traces looks as follow:
The source always resetting its power after the source capabilities are recieved. And the board restarts.
Any ideas how to fix this?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-11 3:01 AM
Hi @BoSt
I assume the sink cannot evaluate the received source capabilities to determine the best power profile to request.
Did you check user code section dedicated for evaluating capabilities
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-11 12:16 PM
Thanks, for reply!
I have tried both the:
void USBPD_DPM_SNK_EvaluateCapabilities(uint8_t PortNum, uint32_t *PtrRequestData, USBPD_CORE_PDO_Type_TypeDef *PtrPowerObjectType)
{
/* USER CODE BEGIN USBPD_DPM_SNK_EvaluateCapabilities */
USBPD_USER_SERV_EvaluateCapa(PortNum, PtrRequestData, PtrPowerObjectType);
}
and the code from the example:
void USBPD_DPM_SNK_EvaluateCapabilities(uint8_t PortNum, uint32_t *PtrRequestData, USBPD_CORE_PDO_Type_TypeDef *PtrPowerObjectType)
{
/* USER CODE BEGIN USBPD_DPM_SNK_EvaluateCapabilities */
uint32_t *srcPDOs;
uint32_t srcPDOCount;
// Retrieve Source PDOs for evaluation
USBPD_PWR_IF_GetPortPDOs(PortNum, USBPD_CORE_DATATYPE_SRC_PDO, (uint8_t*)&srcPDOs, &srcPDOCount);
USBPD_SNKRDO_TypeDef rdo;
/* Initialize RDO */
rdo.d32 = 0;
/* Prepare the requested pdo */
rdo.FixedVariableRDO.ObjectPosition = 0;
rdo.FixedVariableRDO.OperatingCurrentIn10mAunits = 50;
rdo.FixedVariableRDO.MaxOperatingCurrent10mAunits = 50;
rdo.FixedVariableRDO.CapabilityMismatch = 0;
*PtrPowerObjectType = USBPD_CORE_PDO_TYPE_FIXED;
*PtrRequestData = rdo.d32;
/* USER CODE END USBPD_DPM_SNK_EvaluateCapabilities */
}
with the same results. The board are still resetting!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-11 2:21 PM
Hi @BoSt
Is PPS Programmable power supply activated? Could it be disabled for test? Would you share minimal project to reproduce?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-13 12:30 PM - edited ‎2024-11-13 1:01 PM
No, i dont think its activated!
I have a minimal project with just one task blinking a LED. The MX_USBPD_Init(); are hanging up the program and not even the blink task is starting after the board has reset.
On my test board the UCPD1_CC1 and UCPD1_CC2 are connected directly to the USB-C connector and VBUS connected to a voltage regulator.
Thanks!