2022-02-23 2:18 AM
Hello,
I would like to know how to prevent the execution of the on chip bootloader after a RDP regression from level 1 to level 0. After the necessary option byte load (OBL) a mass erase is done and the chip is reset and after the reset the bootloader is executed.
Since I am programming all option bytes, I have played with different values for option bits nBOOT0, nBOOT1 and nBOOT_SEL but no combination will do the trick...
Thank you!
Solved! Go to Solution.
2022-03-04 1:50 AM
I discovered a little trick to circumvent the problem: I just program the bits nBOOT0, nBOOT1 and nBoot_SEL bits to select boot from SRAM before doing the RDP regression. This bypasses the empty check and prevents bootloader execution successfully. After flash programming is complete, I just reprogram those bits to select boot from flash and that's it ;)
2022-02-23 2:39 AM
> after a RDP regression from level 1 to level 0
How do you do that?
> After the necessary option byte load (OBL) a mass erase is done and the chip is reset
'G0B0 implements the FLASH empty check/AN2606 pattern 11 bootloader entry. So either program the FLASH immediately after the bulkerase, without reset; or set the option bits influencing bootloader entry so that they prevent bootoader entry upon empty flash.
JW
2022-02-23 2:50 AM
2022-02-23 3:37 AM
Well STM32G0B0 doesn't have the FLASH_SECR register, so no BOOT_LOCK available. That was the first thing I checked... ;)
2022-02-23 3:53 AM
> How do you do that?
I'm using SEGGER J-Flash utility together with Flasher ATE programmer. With this you can define init and exit steps for programming the target. Im doing the regression in the init steps:
The bootloader is active between the last two steps.
With these steps I can change the option bits FLASH_OPTR::nBOOT0, FLASH_OPTR::nBOOT1 and FLASH_OPTR::nBOOT_SEL, but none of the 8 possible combinations prevent the bootloader from executing!
2022-02-23 4:58 AM
Then there's probably no other way than to program the first word of FLASH to non-FFFFFFFF.
JW
2022-02-23 5:10 AM
Well, the flash will be programmed after finishing the init steps anyway, but between two of those init steps (see my other post: between OBL and reset and hold) the bootloader is active. That is what I'm trying to prevent. The bootloader is not running after the reset and hold step...
2022-02-23 5:20 AM
IMO you should be able to perform all these operations while being under reset all the time, but I am no expert on the boot sequence. You should perhaps talk to Segger.
JW
2022-03-04 1:50 AM
I discovered a little trick to circumvent the problem: I just program the bits nBOOT0, nBOOT1 and nBoot_SEL bits to select boot from SRAM before doing the RDP regression. This bypasses the empty check and prevents bootloader execution successfully. After flash programming is complete, I just reprogram those bits to select boot from flash and that's it ;)
2022-03-04 9:23 AM
Interesting trick, thanks for sharing.
JW