2021-02-25 4:21 AM
I am new to LWIP and MQTT. I am trying to use MQTT using LWIP in stm32f767 . I am able to get ethernet connection up and ping also works. I use mqtt_client_connect to connect to the server. The function is as follows:-
mqtt_client_connect(mqtt_client_t *client, const ip_addr_t *ip_addr, u16_t port, mqtt_connection_cb_t cb, void *arg,const struct mqtt_connect_client_info_t *client_info)
{{
err_t err;
size_t len;
u16_t client_id_length;
/* Length is the sum of 2+"MQTT", protocol level, flags and keep alive */
u16_t remaining_length = 2 + 4 + 1 + 1 + 2;
u8_t flags = 0, will_topic_len = 0, will_msg_len = 0;
LWIP_ASSERT("mqtt_client_connect: client != NULL", client != NULL);
LWIP_ASSERT("mqtt_client_connect: ip_addr != NULL", ip_addr != NULL);
LWIP_ASSERT("mqtt_client_connect: client_info != NULL", client_info != NULL);
LWIP_ASSERT("mqtt_client_connect: client_info->client_id != NULL", client_info->client_id != NULL);
if (client->conn_state != TCP_DISCONNECTED) {
LWIP_DEBUGF(MQTT_DEBUG_WARN,("mqtt_client_connect: Already connected\n\r"));
return ERR_ISCONN;
}
/* Wipe clean */
memset(client, 0, sizeof(mqtt_client_t));
client->connect_arg = arg;
client->connect_cb = cb;
client->keep_alive = client_info->keep_alive;
mqtt_init_requests(client->req_list);
/* Build connect message */
if (client_info->will_topic != NULL && client_info->will_msg != NULL) {
flags |= MQTT_CONNECT_FLAG_WILL;
flags |= (client_info->will_qos & 3) << 3;
if (client_info->will_retain) {
flags |= MQTT_CONNECT_FLAG_WILL_RETAIN;
}
len = strlen(client_info->will_topic);
LWIP_ERROR("mqtt_client_connect: client_info->will_topic length overflow", len <= 0xFF, return ERR_VAL);
LWIP_ERROR("mqtt_client_connect: client_info->will_topic length must be > 0", len > 0, return ERR_VAL);
will_topic_len = (u8_t)len;
len = strlen(client_info->will_msg);
LWIP_ERROR("mqtt_client_connect: client_info->will_msg length overflow", len <= 0xFF, return ERR_VAL);
will_msg_len = (u8_t)len;
len = remaining_length + 2 + will_topic_len + 2 + will_msg_len;
LWIP_ERROR("mqtt_client_connect: remaining_length overflow", len <= 0xFFFF, return ERR_VAL);
remaining_length = (u16_t)len;
}
/* Don't complicate things, always connect using clean session */
flags |= MQTT_CONNECT_FLAG_CLEAN_SESSION;
len = strlen(client_info->client_id);
LWIP_ERROR("mqtt_client_connect: client_info->client_id length overflow", len <= 0xFFFF, return ERR_VAL);
client_id_length = (u16_t)len;
len = remaining_length + 2 + client_id_length;
LWIP_ERROR("mqtt_client_connect: remaining_length overflow", len <= 0xFFFF, return ERR_VAL);
remaining_length = (u16_t)len;
if (mqtt_output_check_space(&client->output, remaining_length) == 0) {
return ERR_MEM;
}
client->conn = tcp_new();
if (client->conn == NULL) {
return ERR_MEM;
}
/* Set arg pointer for callbacks */
tcp_arg(client->conn, client);
/* Any local address, pick random local port number */
err = tcp_bind(client->conn, IP_ADDR_ANY, 0);
if (err != ERR_OK) {
LWIP_DEBUGF(MQTT_DEBUG_WARN,("mqtt_client_connect: Error binding to local ip/port, %d\n\r", err));
goto tcp_fail;
}
LWIP_DEBUGF(MQTT_DEBUG_TRACE,("mqtt_client_connect: Connecting to host: %s at port:%"U16_F"\n\r", ipaddr_ntoa(ip_addr), port));
/* Connect to server */
err = tcp_connect(client->conn, ip_addr, port, mqtt_tcp_connect_cb);
if (err != ERR_OK) {
LWIP_DEBUGF(MQTT_DEBUG_TRACE,("mqtt_client_connect: Error connecting to remote ip/port, %d\n\r", err));
goto tcp_fail;
}
/* Set error callback */
tcp_err(client->conn, mqtt_tcp_err_cb);
client->conn_state = TCP_CONNECTING;
/* Append fixed header */
mqtt_output_append_fixed_header(&client->output, MQTT_MSG_TYPE_CONNECT, 0, 0, 0, remaining_length);
/* Append Protocol string */
mqtt_output_append_string(&client->output, "MQTT", 4);
/* Append Protocol level */
mqtt_output_append_u8(&client->output, 4);
/* Append connect flags */
mqtt_output_append_u8(&client->output, flags);
/* Append keep-alive */
mqtt_output_append_u16(&client->output, client_info->keep_alive);
/* Append client id */
mqtt_output_append_string(&client->output, client_info->client_id, client_id_length);
/* Append will message if used */
if ((flags & MQTT_CONNECT_FLAG_WILL) != 0) {
mqtt_output_append_string(&client->output, client_info->will_topic, will_topic_len);
mqtt_output_append_string(&client->output, client_info->will_msg, will_msg_len);
}
return ERR_OK;
tcp_fail:
tcp_abort(client->conn);
client->conn = NULL;
return err;
}
Here we need to pass IP address of the server to which we want to connect. I want to use hostname instead of IP address. What changes will i need to do so that it takes the hostname like "broker.mqttdashboard.com" ??
Thank you for the help.
Solved! Go to Solution.
2021-03-16 3:22 AM
MEM_SIZE configured in the device is 2000. should I increase it? the data which I am sending is "Hello World", only 11 bytes.
2021-03-16 3:23 AM
I am compiling in keil and heap size is 0x4000
2021-03-16 9:59 AM
Hello
cubemx memory settings are very conservative and guarantee the min functionality (ICMP and small tcp/udp packets)
Try, as an emergency workaround, not optimized: (assuming that use CUBEMX)
increase segment size TCP_MSS to 1460 (this is max for ethernet)
increase PBUF_POOL_BUFSIZE to 1600 (mss+headers+etc) Send buffer (TCP_SND_BUF) will increase automatically.
and MEM_SIZE to 16000 (it seems too high but trimming is a time consuming procedure. Make it after, when project is operative)
2021-03-16 1:58 PM
The PBUF_POOL_BUFSIZE is also adjusted automatically by default:
#define PBUF_POOL_BUFSIZE LWIP_MEM_ALIGN_SIZE(TCP_MSS+40+PBUF_LINK_ENCAPSULATION_HLEN+PBUF_LINK_HLEN)Also take a note that if MEM_USE_POOLS (recommended) or MEM_LIBC_MALLOC (rarely) is enabled, then lwIP integrated heap is not used and MEM_SIZE value doesn't matter.
2021-03-17 3:57 AM
.
2021-03-17 5:28 AM
Thank you @Vangelis Fortounas I defined buffer length as you suggested and now the OUT of memory error is gone. It goes ahead and shows that it is sending tcp data but I doubt if its actually sending coz I am not observing the data on my server.
MX_LWIP_Init
netif: netmask of interface set to 255.255.255.0
netif: GW address of interface set to 192.168.1.1
netif_set_ipaddr: netif address being changed
netif: IP address of interface set to 192.168.1.120
netif: added interface st IP addr 192.168.1.120 netmask 255.255.255.0 gw 192.168.1.1
netif: setting default interface st
netlink is up
tcp_bind: bind to port 80
httpd_init
myCGIinit
IP resolved is 43.61.0.8
inside example_do_connect
tcp_bind: bind to port 49153
mqtt_client_connect: Connecting to host: 43.61.0.8 at port:18973
tcp_connect to port 18973
tcp_enqueue_flags: queueing 6509:6510 (0x2)
tcp_output_segment: 6509:6509
mqtt_publish: Publish with payload length 15 to topic "aeplIN/sidabc/test2"
mqtt_output_send
ringbuf_lin_len 88... send_len 2920
mqtt_output_send: tcp_sndbuf: 2920 bytes, ringbuf_linear_available: 88, get 0, put 88
wrap
tcp_write(pcb=20008640, data=200045c0, len=88, apiflags=1)
tcp_pbuf_prealloc
tcp_write: queueing 6510:6598
tcp_output flush
Publish Success.
2021-03-17 5:30 AM
@Piranha I guess increasing MEM size solved the issue. Thank you :)
2021-03-17 10:19 PM
.
2021-03-25 11:32 PM
Hello @sne_123 I am having DNS problem in my code. Could you please share What steps you followed to resolve DNS problem.
I can not get proporly resolved DNS address in callback function.
2021-03-26 3:00 AM
@voyvoda . Hello... As the above mentors suggested LWIP_DNS need to be be defined as 1 inside lwipopts.h to use DNS functionality. (#define LWIP_DNS 1)
Have you set the dns server ip address?? Even I had this issue but dns got resolved after I added proper dns server address...I am using code below:-
dns_init();
ip_addr_t primaryDnsServer;
ip4_addr_set_u32(&primaryDnsServer, ipaddr_addr("192.168.0.1")); // here set your dns server address
dns_setserver(0, &primaryDnsServer);
char* dnsname = "www.freertos.com";
ip_addr_t dnsresp;
dns_gethostbyname(dnsname, &dnsresp, dns_found, 0);
dns_found(dnsname, &dnsresp, 0);
and my dns_found is callback here:-
void dns_found(const char *name, ip_addr_t *addr, void *arg)
{
char ip_string[20];char* token1;
LWIP_UNUSED_ARG(arg);
printf("%s: %s\n", name, addr ? ip_ntoa(addr) : "<not found>");
sprintf(ip_string,"%s",addr ? ip_ntoa(addr): "<not found>");
printf("ip_string is %s\n\r",ip_string);
}