cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f7508-DK Audio save in SD card example

Ss.61
Associate III

I am using stm32f7508-DK

Try to save Audio in SD card

Please suggest the related example will help me to complete the task.

regards

siva

2 REPLIES 2

As far as the SD Card is concerned, it's just a file - no different to any other file.

SD Card examples should be easy to find...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thank you very much for your quick reply,

My concern is in Firmware package (example)

Two Different examples 1.Audio record 2.Fatfsusd

i want to combine those 2 examples

when i try to combine some of the dependency files (header files are not added )

for example i add Stm32fxx_hal_sd.c in Audio Record example (required Stm32fxx_hal_sd.h file is not appear)

kindly help to figure out the problem

thanks

siva