2019-07-27 5:32 AM
Hi!
I am using stm32f723 to implement usb device mass storage.
I try to mass storage using an internal flash, but I get a message that the formatting is not complete.
I have developed it by referring to the link below, and I have confirmed the same value for reading and writing.
But it is doesn't working.
Can someone please confirm?
I put the file in the attachment.
2019-07-27 6:03 AM
The large flash sectors, and erase times, make the internal flash of the F7 series ill suited to a FAT/MSC solution. Consider external flash memories with smaller erase block sizes, eMMC chips designed for such tasks.
2019-07-27 7:01 AM
Thank you.
The test product does not have an emmc or nand, so I'm testing it with an internal flash to check some actions.
2019-07-27 7:09 AM
Then you'll need to manage the deblocking and partial writes to flash sectors holding existing data.
2019-07-27 4:48 PM
Thank you.
I'll try it.