2023-06-20 2:31 AM - last edited on 2023-06-27 1:59 AM by Amel NASRI
I am getting not able to read usb joystick(Logitech ThrustMaster), callback called to 2 times only. after that there is no call.
void USBH_HID_EventCallback(USBH_HandleTypeDef *phost){
}
How to resolve this issue, i am using repository https://github.com/dong-higenis/stm32f401ccu_usb_host_ps3_joystick , which created by some other user. can someone help to resolve this issue? If you are able to read, can you provide me link to example code?
If I use china made joystick, I am getting USBH_NOT_SUPPORTED on setting HID set protocol.
case HID_REQ_SET_PROTOCOL:
/* set protocol */
classReqStatus = USBH_HID_SetProtocol(phost, 0U);
if (classReqStatus == USBH_OK)
{
HID_Handle->ctl_state = HID_REQ_IDLE;
/* all requests performed*/
phost->pUser(phost, HOST_USER_CLASS_ACTIVE);
status = USBH_OK;
}
else if (classReqStatus == USBH_NOT_SUPPORTED)
{
USBH_ErrLog("Control error: HID: Device Set protocol request failed");
status = USBH_FAIL;
}
else
{
/* .. */
}
break;
Can some help me to resolve this issue?