2014-06-20 3:53 AM
Hello everybody.
I am working in a project withhttp://www.st.com/web/catalog/mmc/FM141/SC1169/SS1577/LN1789/PF253733?s_searchtype=partnumber
connected to ahttp://www.micrel.com/index.php/products/lan-solutions/ieee-1588/article/1-ksz8463ml.html
Ethernet transceiver, via MII interface. I am experimenting some trouble with the transmission data pins from STM32F4 (TXD0-3). With an oscilloscope, I have tested this pins and the signal is always the same (and wrong). Reception pins work fine. Also I have tested the same source code with an STM32F4 evaluation board, and all work OK. I wonder if anyone has had similar problems with Ethernet MII connection. Thank you. #mii-ethernet-waveform #stm32f4-micrel-ethernet-mii2014-06-20 5:03 AM
Issues with Ethernet PHYs usually come down to a couple of things:
Pin configurations and connection. Clock speeds, routing, expectations. PHY configuration address, and internal configuration. I don't see any code or schematics, and don't really know what ''wrong'' means in this context. Suggest you look at other STM32 designs that have used this Micrel part successfully.2014-06-21 3:47 AM
Hello.
At this moment I can't access to the physical device to get the waveforms from the MII interface. I will check these points and I'm trying to upload more information on Monday. Regards, Jose A.2014-06-23 2:47 AM
Functions inside stm32f4x7_eth_bsp.c:
void
ETH_BSP_Config(
void
)
{
RCC_ClocksTypeDef RCC_Clocks;
/***************************************************************************
NOTE:
When using Systick to manage the delay in Ethernet driver, the Systick
must be configured before Ethernet initialization and, the interrupt
priority should be the highest one.
*****************************************************************************/
/* Configure Systick clock source as HCLK */
SysTick_CLKSourceConfig(SysTick_CLKSource_HCLK);
/* SystTick configuration: an interrupt every 10ms */
RCC_GetClocksFreq(&RCC_Clocks);
/* Wait until SysTick configuration be successful */
while
(SysTick_Config(RCC_Clocks.HCLK_Frequency / 100) != 0) {
}
/* Set Systick interrupt priority */
NVIC_SetPriority (SysTick_IRQn, 1);
/* Configure the GPIO ports for ethernet pins */
ETH_GPIO_Config();
/* Configure the Ethernet MAC/DMA */
ETH_MACDMA_Config();
/* Init comm with switch */
GPIO_ResetBits(GPIOG, GPIO_Pin_8);
// KSZ8463 Power-down (PWRDN, #17)
GPIO_ResetBits(GPIOG, GPIO_Pin_7);
// KSZ8463 Active reset (RSTN, #63)
Delay(5);
// Wait for switch reset
GPIO_SetBits(GPIOG, GPIO_Pin_8);
// KSZ8463 Normal operation (PWRDN, #17)
GPIO_SetBits(GPIOG, GPIO_Pin_7);
// KSZ8463 Stop reset (RSTN, #63)
Delay(10);
// Wait for switch initialization
printf
(
''CIDER - 0x%
X''
,KSZ_Read(CIDER, 2));
// Check the CIDER register value
if
(EthInitStatus == 0){
LOGERROR(
''Ethernet Init failed, check cable connection
''
);
while
(1);
}
}
static
void
ETH_MACDMA_Config(
void
)
{
ETH_InitTypeDef ETH_InitStructure;
/* Reset ETHERNET on AHB Bus */
ETH_DeInit();
/* Software reset */
ETH_SoftwareReset();
// MUST be BEFORE Ethernet clock enabling !
/* Wait for software reset */
while
(ETH_GetSoftwareResetStatus() == SET);
/* Enable ETHERNET clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_ETH_MAC | RCC_AHB1Periph_ETH_MAC_Tx |
RCC_AHB1Periph_ETH_MAC_Rx, ENABLE);
/* ETHERNET Configuration --------------------------------------------------*/
/* Call ETH_StructInit if you don't like to configure all ETH_InitStructure parameter */
ETH_StructInit(�?_InitStructure);
/* Fill ETH_InitStructure parametrs */
/*------------------------ MAC -----------------------------------*/
ETH_InitStructure.ETH_AutoNegotiation = ETH_AutoNegotiation_Enable;
// ETH_InitStructure.ETH_AutoNegotiation = ETH_AutoNegotiation_Disable;
// ETH_InitStructure.ETH_Speed = ETH_Speed_10M;
// ETH_InitStructure.ETH_Mode = ETH_Mode_FullDuplex;
ETH_InitStructure.ETH_LoopbackMode = ETH_LoopbackMode_Disable;
ETH_InitStructure.ETH_RetryTransmission = ETH_RetryTransmission_Disable;
ETH_InitStructure.ETH_AutomaticPadCRCStrip = ETH_AutomaticPadCRCStrip_Disable;
ETH_InitStructure.ETH_ReceiveAll = ETH_ReceiveAll_Disable;
ETH_InitStructure.ETH_BroadcastFramesReception = ETH_BroadcastFramesReception_Enable;
ETH_InitStructure.ETH_PromiscuousMode = ETH_PromiscuousMode_Disable;
ETH_InitStructure.ETH_MulticastFramesFilter = ETH_MulticastFramesFilter_Perfect;
ETH_InitStructure.ETH_UnicastFramesFilter = ETH_UnicastFramesFilter_Perfect;
#ifdef CHECKSUM_BY_HARDWARE
ETH_InitStructure.ETH_ChecksumOffload = ETH_ChecksumOffload_Enable;
#endif
/*------------------------ DMA -----------------------------------*/
/* When we use the Checksum offload feature, we need to enable the Store and Forward mode:
the store and forward guarantee that a whole frame is stored in the FIFO, so the MAC can insert/verify the checksum,
if the checksum is OK the DMA can handle the frame otherwise the frame is dropped */
ETH_InitStructure.ETH_DropTCPIPChecksumErrorFrame = ETH_DropTCPIPChecksumErrorFrame_Enable;
ETH_InitStructure.ETH_ReceiveStoreForward = ETH_ReceiveStoreForward_Enable;
ETH_InitStructure.ETH_TransmitStoreForward = ETH_TransmitStoreForward_Enable;
ETH_InitStructure.ETH_ForwardErrorFrames = ETH_ForwardErrorFrames_Disable;
ETH_InitStructure.ETH_ForwardUndersizedGoodFrames = ETH_ForwardUndersizedGoodFrames_Disable;
ETH_InitStructure.ETH_SecondFrameOperate = ETH_SecondFrameOperate_Enable;
ETH_InitStructure.ETH_AddressAlignedBeats = ETH_AddressAlignedBeats_Enable;
ETH_InitStructure.ETH_FixedBurst = ETH_FixedBurst_Enable;
ETH_InitStructure.ETH_RxDMABurstLength = ETH_RxDMABurstLength_32Beat;
ETH_InitStructure.ETH_TxDMABurstLength = ETH_TxDMABurstLength_32Beat;
ETH_InitStructure.ETH_DMAArbitration = ETH_DMAArbitration_RoundRobin_RxTx_2_1;
/* Configure Ethernet */
EthInitStatus = ETH_Init(�?_InitStructure, _PHY_ADDRESS);
}
void
ETH_GPIO_Config(
void
)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIOs clocks */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB |
RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOI |
RCC_AHB1Periph_GPIOG | RCC_AHB1Periph_GPIOH |
RCC_AHB1Periph_GPIOF, ENABLE);
/* Enable SYSCFG clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
/* Configure MCO (PA8) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* MII/RMII Media interface selection --------------------------------------*/
#ifdef MII_MODE /* Mode MII with STM324xG-EVAL */
#ifdef PHY_CLOCK_MCO
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Output HSE clock (25MHz) on MCO pin (PA8) to clock the PHY */
RCC_MCO1Config(RCC_MCO1Source_HSE, RCC_MCO1Div_1);
#endif /* PHY_CLOCK_MCO */
SYSCFG_ETH_MediaInterfaceConfig(SYSCFG_ETH_MediaInterface_MII);
#elif defined RMII_MODE /* Mode RMII with STM324xG-EVAL */
SYSCFG_ETH_MediaInterfaceConfig(SYSCFG_ETH_MediaInterface_RMII);
#endif
/* Ethernet pins configuration ************************************************/
/* STM3240-EVAL DISCOVERY/My device
ETH_MDIO -------------------------> PA2 PA2 Not connected
ETH_MDC --------------------------> PC1 PC1 Not connected
ETH_PPS_OUT ----------------------> PB5 ---
ETH_MII_CRS ----------------------> PH2 PA0/WKU
ETH_MII_COL ----------------------> PH3 PA3
ETH_MII_RX_ER** ------------------> PI10 PB10
ETH_MII_RXD2 ---------------------> PH6 PB0
ETH_MII_RXD3 ---------------------> PH7 PB1
ETH_MII_TX_CLK -------------------> PC3 PC3
ETH_MII_TXD2 ---------------------> PC2 PC2
ETH_MII_TXD3 ---------------------> PB8 PE2
ETH_MII_RX_CLK/ETH_RMII_REF_CLK---> PA1 PA1
ETH_MII_RX_DV/ETH_RMII_CRS_DV ----> PA7 PA7
ETH_MII_RXD0/ETH_RMII_RXD0 -------> PC4 PC4
ETH_MII_RXD1/ETH_RMII_RXD1 -------> PC5 PC5
ETH_MII_TX_EN/ETH_RMII_TX_EN -----> PG11 PB11
ETH_MII_TXD0/ETH_RMII_TXD0 -------> PG13 PB12
ETH_MII_TXD1/ETH_RMII_TXD1 -------> PG14 PB13
** bypass mode control
*/
/* Configure PA0, PA1, PA2, PA3 and PA7 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 |GPIO_Pin_1 |
/* GPIO_Pin_2 |*/
GPIO_Pin_3 | GPIO_Pin_7;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_ETH);
// GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_ETH);
/* Configure PB0, PB1, PB10, PB11, PB12 and PB13 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_10 |
GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 ;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource0, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource1, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_ETH);
/* Configure PC1, PC2, PC3, PC4 and PC5 */
GPIO_InitStructure.GPIO_Pin =
/*GPIO_Pin_1 |*/
GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5;
GPIO_Init(GPIOC, &GPIO_InitStructure);
// GPIO_PinAFConfig(GPIOC, GPIO_PinSource1, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource2, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource3, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource4, GPIO_AF_ETH);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource5, GPIO_AF_ETH);
/* Configure PE2 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource2, GPIO_AF_ETH);
}
I am using MII_MODE with NO PHY_CLOCK_MCO. Also my pin configuration is like the discovery board (second column in
ETH_GPIO_Config
function).
When I run the program, I can read from KSZ transceiver the information (CIDR = 0x8443) which is OK.
I attach screenshots from the transmission related pins. The waveform of TXD0, TXD1, TXD2 and TXD3 is always the same and it doesn't change.
2014-06-23 8:22 AM
Problem
SOLVED
. I will try to explain what was the solution.2015-09-14 10:21 PM
My STM32F4 shows the exactly same unwanted waveforms on TXD[3:0] in MII Mode. The width of TXEN signal shows also only 600~700 nsec as you have observed. Please share your valuable solution.