2017-06-28 11:56 AM
Hello all,
I am having a difficulty trying to get my STM32F411E-DISCO board to go into DFU mode. After applying power to the mini USB connector (USB ST-LINK), the default program operates. I then want to go into DFU mode so I have the the power cable in the mini USB and a micro USB plugged in for the DFU and I bridge BOOT0 to VDD with a jumper and press RESET and the board will not connect to DFU. All that happens is the main demo program stops operating. Any insight as to why this is happening? I did the exact same thing on my STM32F407G-DISC1 and I can get to DFU without any issue.
Any help that can be given will be greatly appreciated. Thank you in advance.
#stm32f411e-disco #dfu #stm32f407g-disc1 #dfu-bootloaderSolved! Go to Solution.
2017-06-29 8:09 AM
Hi All,
I discovered the reason for the error. The
STM32F411E-DISCO
was missing the solder bridge (SB20) that pulled PB2 to a low state. Putting the jumper on PB2 made it work. ^-^vHope this will help someone else with a similar issue.
2017-06-29 8:09 AM
Hi All,
I discovered the reason for the error. The
STM32F411E-DISCO
was missing the solder bridge (SB20) that pulled PB2 to a low state. Putting the jumper on PB2 made it work. ^-^vHope this will help someone else with a similar issue.
2020-06-15 5:35 AM
Thanks Aron,
This was useful! Faced exactly same issue, on exactly same board and the jumper from PB2 to GND fixed it.