cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f411e-disco bootloader Usart1

OTofa.1
Associate

Hi

I am trying unsuccessfully to use the flash loader demostrator to load the new firmwire.

I have pinned the Boot1 (0 to gnd) and Boot0 (1 to vdd) pins.

For the application (Flash loader demostrator I set the parity even, data bit 8 and speed 115200. I tried other speeds without any success.

I use an mcp2200 as usb-uart interface.

I tried to enter DFU mode and I managed it without any problems.

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Check schematic, the is a large capacitor related to the USB interface on the USART1 PA9/PA10 pins which interferes.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi

I removed the capacitor, now the stm32cubeprogrammer software tells me this.

16:53:28 : Serial Port COM6 is successfully opened.

16:53:28 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off

16:53:28 : Activating device: OK

16:53:28 : Chip ID: 0x431 

16:53:28 : BootLoader protocol version: 3.1

16:53:29 : Response received from device: NACK

16:53:29 : Error: GETID command not acknowledged!

16:53:29 : Reemission of GetID command

16:53:31 : Response received from device: NACK

16:53:31 : Error: READ command not acknowledged at address: 0x1FFFC008

16:53:32 : Response received from device: NACK

16:53:32 : Error: READ command not acknowledged at address: 0x1FFF7A22

16:53:34 : UPLOADING OPTION BYTES DATA ...

16:53:34 : Bank : 0x00

16:53:34 : Address : 0x1fffc000

16:53:34 : Size : 16 Bytes

16:53:34 : Response received from device: NACK

16:53:34 : Error: READ command not acknowledged at address: 0x1FFFC000

16:53:34 : Error: Uploading Option Bytes bank: 0 failed

16:53:34 : Error: Initializing the Option Bytes failed

16:53:34 : Disconnected from device.