cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411CEU6 via STLINK V2 - C13 (Board LED: on/off) - configuration check under Linux with stlink-gui failed

timbo2023
Associate III

Hi there,

 

 

follow the attached picture, an easy question for you, for me an effort.

 

left side:

Compiling procedure for a simple 32-bit binary file, ARM

right side:

program code - board LED should turn on

result:

turn on LED - failed

 

Questions:

A

In my opinion it is a failure regarding the "header-handling".

I work with the present CMSIS-files.

Are there hints to integrate the header in a right way?

Are there program failures?

B

Do you know an exactly openocd-instruction to reach the same result as with stlink-gui?

 

 

Regards,

timbo2023

1 REPLY 1
Saket_Om
ST Employee

Hello @timbo2023 

Which compiler you are using please? 

>>Do you know an exactly openocd-instruction to reach the same result as with stlink-gui?

I recommend using the STM32Cube programmer to flash your MCU.

 

 

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar