2022-03-12 02:46 PM
Here's the code of my app_threadx.c file.
I followed the STM32 AZURE RTOS workshop for the H7 MCUs, however, I'm currently developing on a STM32F401RE.
Basically, when I debug the program the function it's called and then go to sleep, despite the fact of it doesn't wake up, so it doesn't work as a thread anymore.
I don't know if there's any timer problem, I've set TIM10 as timebase source because I can't use the SysTick due STM software constraints (to avoid any conflict with the SysTick interrupt handler).
I think it could be a library problem, however I don't know what can I do except these basic things.
Thanks in advance!
2022-03-16 01:52 AM
Hello @f4_kiddo ,
You can refer to the following example provided under X-Cube-AZRTOS-F4 Package:
I hope this helps.
BeST Regards,
Walid
2022-03-28 02:48 AM
Thanks, I will report the solution found by @KR51K :
I think I found the answer: in my project the Priority Group in "System Core"->"NVIC" was set to "0 bits", so I changed his to "4 bits". and afterwards set the "Preemption Priotity" for the "Time base: TIM6 global interrupt..." from "0" to "15".
Hope this helps you
Basically this was the only setting that was missing in my project.