cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4-discovery with STM32CubeMX

ilias
Associate II
Posted on January 16, 2015 at 06:58

Hello,

I am using an

stm32f4-discovery

board with MCU

stm32F407

.

My intention is create a project using the

STM32CubeM

X c generator using both RTOS and USB Middlewares. I want to be able to see in my Device Manager of my PC a new HID device when I connect the board using the micro usb connector.

My problem is that although the project is created normally is built successfully using IAR workbench, finally no HID device is identified.

I have enabled in the peripherals of the board USB_OTG_HS as device and I have set the Middleware USB Device class as HID.

I have also tried other combinations (I also USB_OTG_FS) but no result.

I am newbie and what I am asking is if anybody knows how to enable the usb and rtos using the CubeMX c code generator.

Thanks in advance.

#stm32f4-discovery-usb-cube
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
ST Employee
Posted on March 23, 2015 at 13:37

Please use .ioc file attached to generate your project.

Ensure heap/stack sizes for your project are sufficient:in IAR IDE, right click project name and select Options > Linker > Config -> Override default. thenEdit>Stack/Heap sizessettingsTab.

Set 0x2000 for both.

________________

Attachments :

DiscoF407_USBDeviceHID.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzNm&d=%2Fa%2F0X0000000bLM%2FVFIHAbC8A1oddO9c9pc3dvDPAfRLhl.yjpyYfA1iYlU&asPdf=false