2013-04-30 5:30 AM
Hi,
I was looking for USB CDC (Virtual COM) Example code for STM32F3DISCOVERY Kit.I can't see it in Example code downloaded from ST.Regards, #usb-(cdc) #stm32f3-discovery-usb-cdc-web #amazing-google-skills2014-09-15 2:24 AM
how do I port to stm32f3 discovery? could you help me out with this?
2014-09-15 5:46 AM
how do I port to stm32f3 discovery? could you help me out with this?
You look at the reference examples, and you adapt them to the specifics of the board you are using. If you don't know the differences, then start there.2014-12-07 2:21 AM
Good Morning. Thank you in advance for any advice.
I would like to realize the communication USB CDC ( virtual com ) , the example set by St. , creates the virtual device and the PC recognizes it . But how do I write in the virtual com port and send the data to my PC ? how do I read data coming back from the PC ? I am a student of the University of Palermo , novice with ARM . I can handle all of the board thanks to numerous examples given by ST. Except this communication , essential to collect data for my thesis . The alternative would implement UART and build a hardwar with max 232 , but I would avoid , as the card has the ability to communicate directly with the PC. Thanks in advance . The ideal sarebe to have an example of eco com , possibly in keil .2016-07-25 9:43 AM
Tags: amazing Google skills. LOL.