cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F3DISCOVERY USB CDC (Virtual COM port) Example

harshad
Associate II
Posted on April 30, 2013 at 14:30

Hi,

I was looking for USB CDC (Virtual COM) Example code for STM32F3DISCOVERY Kit.

I can't see it in Example code downloaded from ST.

Regards,

#usb-(cdc) #stm32f3-discovery-usb-cdc-web #amazing-google-skills
13 REPLIES 13
vineet
Associate
Posted on September 15, 2014 at 11:24

how do I port to stm32f3 discovery? could you help me out with this?

Posted on September 15, 2014 at 14:46

how do I port to stm32f3 discovery? could you help me out with this?

You look at the reference examples, and you adapt them to the specifics of the board you are using. If you don't know the differences, then start there.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
giova220389
Associate
Posted on December 07, 2014 at 11:21

Good Morning. Thank you in advance for any advice.

I would like to realize the communication USB CDC ( virtual com ) , the example set by St. , creates the virtual device and the PC recognizes it . But how do I write in the virtual com port and send the data to my PC ? how do I read data coming back from the PC ? I am a student of the University of Palermo , novice with ARM . I can handle all of the board thanks to numerous examples given by ST. Except this communication , essential to collect data for my thesis . The alternative would implement UART and build a hardwar with max 232 , but I would avoid , as the card has the ability to communicate directly with the PC. Thanks in advance . The ideal sarebe to have an example of eco com , possibly in keil .

orhangazi4401
Associate II
Posted on July 25, 2016 at 18:43

Tags: amazing Google skills. LOL.