cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f107 lwip freertos printf problem

Erkan Ersoy
Associate II
Posted on December 19, 2016 at 16:05

Hello;

I am trying to implement FreeRTOS 9.0.0 and lwip2.0.0 with HAL library and GCC

For easiness I generated FreeRTOS code with STM32CubeMX and replaced FreeRTOS to 9.0.0 and then added LWIP. 

I can ping my device without using debug options enabled.

 to use debug output I wrote that write function:

/*Low layer write(output) function*/

__attribute__ ((used))

int _write(int file, char *ptr, int len)

{

HAL_UART_Transmit(&huart5, ptr, len, 0xff);

}

But I had problem with HAL_Delay function and couldn't figure out to get rid of it. (I read tried some solutions but didn't work)

Then I decided if I use write function without HAL_delay may solve my problem so I used :

int _write(int file, char *ptr, int len)

{

int i=0;

/* Transmit Data */

for (i = 0; i < len; i++) {

UART5->DR = (*ptr++ & (uint16_t)0x01FF);

while(UART5->SR & USART_SR_TC_Msk == RESET);

}

But it didn't work. (Didn't stuck either.)

How should I use printf function ?

#stm32f107 #printf #freertos #lwip #debug #usart
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0