2020-11-19 8:18 AM
Hi,
I am at a loss as to why this is not working.
I have checked the crystal (ABM8AIG-8.000MHZ-1Z-T), wiring (1.5k resistor between D+ and 3V3, connected both before and after MX_USB_DEVICE_Init() is called), etc.
I've set the stack/heap sizes to 0x400 (not that this should matter as I'm using static allocation).
I've tried adjusting CDC_DATA_FS_MAX_PACKET_SIZE both bigger and smaller.
Stepping through code I find that the I fail at USBD_GetStatus as the req->wLength is 0.
So somewhere the data is being lost.
Any ideas?
2020-11-19 8:38 AM
OK, so I found a single line in RM0008 (https://www.st.com/resource/en/reference_manual/cd00171190-stm32f101xx-stm32f102xx-stm32f103xx-stm32f105xx-and-stm32f107xx-advanced-armbased-32bit-mcus-stmicroelectronics.pdf) saying that USB and CAN share a dedicated 512-byte SRAM.
I removed my CAN code, and the USB now works!
I guess my next question is, given my project was going to act as an interface between USB and CAN, how do I get CAN working too?