2018-02-21 10:20 AM
Hi,
I've successfully run a FreeRTOS program that use ADC + DMA in scan, continuous, circular mode and I successfully can average in HAL_ADC_ConvCpltCallback().
Now I'd still like to use DMA to fill a buffer of 3 channels x 8 conversions but I'd like to start the conversion from a FreeRTOS software timer.
So I'd expect that I start the DMA from a software timer, once the hardware has finished it stops conversions and HAL_ADC_ConvCpltCallback() get called, I average results and wait another software timer restart the conversion.
I've tried to disable continuous mode, to run DMA in REGULAR mode vs CIRCULAR... but every time I try, the second time HAL_ADC_Start_DMA() get called I get an HAL_ERROR from ADC_Enable().
This works continuously if I just call HAL_ADC_Start_DMA() once.
uint16_t ADCraw[ADCSamples][ADCChannels];
hadc1.Instance = ADC1;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 3;hdma_adc1.Instance = DMA1_Channel1;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE; hdma_adc1.Init.MemInc = DMA_MINC_ENABLE; hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_adc1.Init.Mode = DMA_CIRCULAR; hdma_adc1.Init.Priority = DMA_PRIORITY_LOW;HAL_ADC_Start_DMA(&hadc1, (uint32_t*) ADCraw, ADCChannels * ADCSamples);
Thanks
#freertos #software-timer #stmf1 #continuous-conversion #dma #adc2018-08-10 9:24 AM
Sorry, bumping old zombie unanswered threads off my feed