cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F091 internal bootloader support CAN?

Mat1
Associate III

Hi,

I studied the RM0091 (page 55). There UART, I2C is listed as supported interfaces for the internal bootloader.

I was wondering why the CAN isn't supported. Is this the case?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mat1
Associate III

Yes, it does.

Thank you for the prompt answer.

You're welcome!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Javier1
Principal

Before you happily jump into using the STM canbus bootloader, have it mind it WONT WORK if more than one canbus node is active.

I realiced it the hard way https://community.st.com/s/question/0D53W00000apgoISAQ/is-the-stm-system-bootloader-trough-canbus-just-not-woking-when-more-than-one-device-shares-the-bus

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/