2018-07-04 11:56 PM
Hi all,
I'm having a strange problem with a design using the STM32F072V8 MCU.
MCU operates at 3.3V. We have a USB connector internal to the product, solely for programming the MCU via DFU.
I have the BOOT0 pin connected to VBUS on a USB connector through a resistor divider that means 3.3V is on the BOOT0 pin whenever USB is connected, and the BOOT0 pin is grounded when no USB is connected.
The intended procedure to access the DFU is to:
- Connect USB to host while device is unpowered
- Power up the device
We expect to enter DFU mode since the BOOT0 pin is held high before the system power is up.
Instead of entering DFU mode, I see the following in Linux dmesg:
[28936069] usb 3-13: new full-speed USB device number 49 using xhci_hcd
[28064068] usb 3-13: device descriptor read/64, error -71 [28300075] usb 3-13: device descriptor read/64, error -71 [28536067] usb 3-13: new full-speed USB device number 50 using xhci_hcd [28664084] usb 3-13: device descriptor read/64, error -71 [28900059] usb 3-13: device descriptor read/64, error -71 [28008079] usb usb3-port13: attempt power cycle [28660084] usb 3-13: new full-speed USB device number 51 using xhci_hcd [28660186] usb 3-13: Device not responding to setup address. [28868143] usb 3-13: Device not responding to setup address. [28076066] usb 3-13: device not accepting address 51, error -71 [28204078] usb 3-13: new full-speed USB device number 52 using xhci_hcd [28204178] usb 3-13: Device not responding to setup address. [28412188] usb 3-13: Device not responding to setup address. [28620100] usb 3-13: device not accepting address 52, error -71 [28620142] usb usb3-port13: unable to enumerate USB deviceIf at this point I then assert the NRST line (by shorting NRST to GND), the MCU resets and the DFU happily comes to life.
I've tried to stretch out the NRST by loading a 1uF capacitor on the NRST pin instead of the prescribed 100nF, but I still see the issue.
I've read some stuff regarding pull-ups on the DP pin of the USB, which I don't have on my design, but the datasheet and the bootloader app note both say I don't need a pull-up. Curiously though, the STM32F072-DISCO discovery board has a DP pull-up installed. I don't see any issues with entering DFU mode on the DISCO board.
Can anyone provide any hints here? I'm kinda running out of things to try.
Thanks in advance!
- Josef
#dfu-bootloader Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2019-01-24 1:51 PM
So, I solved the issue a few months ago but have been off work since then.
In my case, I had a flash memory attached to USART1 (or 2, can't remember, but doesn't matter) and another external part accessing the flash during power up. The STM32 is there to load a binary onto the flash during production and would tristate the USART pins during runtime.
Because there was activity (from the other system device trying to access the flash) on the USART pins when BOOT0 was asserted, the STM32 entered it's UART bootloader flow and thus the USB core was never initialised.
The reason the bootloader worked over USB after reseting the STM32 (without interrupting power) was that the external device was no longer accessing the flash after a couple of seconds after power up, so the desired USB boot flow was able to be entered.
Asserting the external device's reset in hardware made sure it never tried to access the flash device until we entered runtime.
2018-07-05 2:07 AM
I have the BOOT0 pin connected to VBUS on a USB connector through a resistor divider that means 3.3V is on the BOOT0 pin whenever USB is connected, and the BOOT0 pin is grounded when no USB is connected.
The intended procedure to access the DFU is to:
- Connect USB to host while device is unpowered
- Power up the device
I guess the mcu is powered parasitically through the BOOT0 pin enough to start working, switch on the DP pullup causing he host to start enumeration, but the power is not sufficient for subsequent proper working
You are not supposed to pull high a pin of an unpowered device.
JW
2018-07-05 2:12 AM
Curiously though, the STM32F072-DISCO discovery board has a DP pull-up installed.
I don't see any DP pullup on the STM32F072-DISCO's schematic in UM1690 (except of the STLink's pullup, R8, switched by a transistor; but that's a different mcu, a 'F103).
2018-07-05 5:16 PM
Ah yes, my mistake, you are correct.
2018-07-05 5:20 PM
I thought this might be an issue too, but I did try manually shorting the BOOT0 pin to the MCUs VCC, and without USB plugged in. I power up and then plug USB in and see the same issue.
I saw some errata for the stm32f070 series that suggested there were some issues with the bootloader firmware for that series, is it possible I'm experiencing the same issues?
2018-07-05 6:05 PM
Then I don't know.
Can't the problem be related to the bootloader falsely entering one of the other modes, due to 'activity' on some of the 'sensitive' pins (e.g. USART1_RX/USART2_RX) upon powerup, caused by some attached circuitry?
JW
2018-07-05 7:13 PM
Yeah, it's a bit of a pickle. I don't see any 'activity' on any of the UART RX pins, and that seems right since I have loads on these pins (pull-ups/downs) for runtime. Both of the UART TX pins drive pull-ups/downs, so those should be fine too.
I've replicated my circuit on a DISCO board with the STM32F072RBT6 device, so the BOOT0 pin is connected to a divider coming from USB VBUS. No problems going into bootloader mode at all.
- Josef
2018-07-05 9:35 PM
Some further information.
I've hooked up an STLink to my design to read out some registers while supposedly in bootloader mode (as in the state where it's not working correctly).
Further:
So for some reason the MCU is not correctly detecting the BOOT0 pin?
2018-07-06 12:55 AM
Bad solder joint on that pin?
JW
2018-07-06 1:00 AM
Check also all power and ground pins, including the analog.
Is there only one power supply regulator, or are there separate power rails?
Anything unusual connected on the reset pin?
JW