cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042 Bootloader activation on Nucleo

harald
Associate III

Hy,

as described and discussed earlier (https://community.st.com/s/question/0D50X00009sWdDqSAK/stm32f042-bootloader-activation) I want to use bootloader mode of STM32F042 to update STM32 firmware in a multi CPU system. I still see this way as very elegant because I do not need to maintain yet another piece of code and it seems quite fail-safe to me.

During implementation on a NUCLEO-F042K6 I run into problems.

To be able to activate bootloader mode on the Nucleo, I solder a wire to SB12 and conect it to "BOOT" output pin of host CPU.

Also I remove SB3 and connect lower pin to TX pin of host CPU

Also I solder a wire to Pin 24 of STM and connect this to RX of host CPU.

When then asserting the boot sequence (NRST = Low, BOOT = High, NRST = High, Send 0x7F over UART) I do not see a response on RX.

 0690X000006CmVFQA0.png

What might be the root cause? Has anyone ever tried to use bootloader with a Nucleo?

Best regards

Harald

0 REPLIES 0