cancel
Showing results for 
Search instead for 
Did you mean: 

How to generate a delay function with a 1 micro second resolution, without affecting the existing HAL_Delay 1 millisecond resolution function.

JBass
Associate

I'm using a STM32F429ZI Nucleo-144, and need a counter/delay function with 1 microsecond resolution, but want to keep the HAL_Delay function at 1 millisecond resolution for other uses.

I'm looking at potentially reconfiguring the SysTick interrupt to 1 microsecond by modifying the call to HAL_SYSTICK_Config, using HAL_SYSTICK_Callback to create a counter with 1 microsecond resolution, and then overloading the weak HAL_Delay function to take the faster SysTick into account and keep it at 1 ms.​  But HAL_SYSTICK_Config is called from SystemClock_Config which is code generated by STM32Core, so it will be overwritten next time I regenerate the project.  Is there a better way to obtain a counter/delay with 1 microsecond resolution?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0