2015-04-15 2:52 AM
Hello,
perhaps I missed something... Is it correct, that the user labels in CubeMX are not used in the generated code? I've seen this in other code configurator tools. I didn't found a way to benefit from the pin definitions in the code, like ''LED_RED''. If this is not implemented, this is a great feature! I know tools which writes a pin definition file with a bunch of defines like PIN_LED_RED_SetHigh(), PIN_LED_RED_Toggle(), PIN_LED_RED_SetAsOutput(), PIN_LED_RED_EnablePullUp() and so on for the correct replacement with the already mapped HAL functions, pins and ports. Thanks for any help. Greetings STM32CubeMX 4.7.0 / HAL F4 1.5.0 / STM32F407 #user-labels #feature #stm32cube #solved2016-10-05 2:06 AM
Hi mk@sch,
Behind Great Clients comes great progress. Thank you for your contribution.-Hannibal-2018-01-09 9:35 PM
I have a colleague using
Version 4.23.0
STM32Cube V1.0
'Lord I don't understand your version numbering scheme.'
He added User Labels to various pins.
These User Labels are visible in the STM32CubeMX Pins/Signals Options... as well as in the GUI around the MCU, and also in the GPIO Pin Configuration of the Configuration Tab.
NONE OF THESE USER LABELS EVER SHOW UP IN THE GENERATED CODE? WHY? I HAD THE IMPRESSION THAT THIS WAS A FEATURE. AM I NOT INTERPRETING WHAT I AM READING HERE?
His development system is Atollic True Studio Version 8.1
2018-02-01 5:40 AM
Hello all,
I think that the first point (raised by
66794
) was answered and solved since a long time ago.
Regarding your post
tomkins.richard
, indeed, user labels are correctly generated. Here, I took an example of STM32F722ZETX with the pin PC13 named Jeanne_GPIO as below :and after generating the code, I can find this user label in the main.c in the GPIO configuration part :
I think that fully answered the initial topic.
If not, could you please be more precise in your request?
BR. Jeanne
2018-02-01 6:58 AM
,
,
I find my user defined names ♯ defined in main.h
2018-03-18 7:07 PM
I'm sorry, I've been away on an extended, well, it's a log story.
In any event, I shall get back to this in the very near future, as my experience was the opposite of yours.