STM32Cube USB CDC Unknown USB Device Descriptor Request Failed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-24 10:38 AM
I have been working on setting up my MCU as a VCP CDC Device using STM32Cube for the past few days. I have studied the STM32Cube USB device library User Manual (UM1734) and have followed the steps outlined in part 7.5.6 which calls on my application to call the function USBD_CDC_Init().
void MX_USB_DEVICE_Init( void ) { /* Init Device Library,Add Supported Class and Start the library*/ USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS); USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC); USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS); USBD_Start(&hUsbDeviceFS); // USBD_CDC_Init called here hUsbDeviceFS.pClass->Init(&hUsbDeviceFS, DEVICE_FS); } I have changed the value of CDC_DATA_HS_MAX_PACKET_SIZE to 256 in usbd_cdc.h as detailed in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/USB%20CDC%20Bug%20in%20CubeMX%20firmware&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx¤tviews=3282]post to ensure that my device data packet size is 64 bytes. #define CDC_DATA_HS_MAX_PACKET_SIZE 256 /* Endpoint IN & OUT Packet size */ I have also ensured that my heap size is changed to the minimum recommended by ST support in another post on this forum, in my .ld file _Min_Heap_Size = 0x0400; /* required amount of heap */ _Min_Stack_Size = 0x0400; /* required amount of stack */ The problem is if I call the function USBD_CDC_Init() the MCU controller is listed as an UnKnown Device by Windows and stopped. If I comment out the call, my MCU is correctly recognised and configured as a VCP device in both Windows and Linux but all subsequent calls to USBD_CDC_SetTxBuffer will fail (HardFaultHandler is called) because the pClassData field of the USB Device handler is never initialized. I am caught between the devil and the deep blue sea, how do I proceeed? I am using a STM32f302k8 and STM32CubeMX version 4.6.0 with FW version 1.1.1 for STM32F3. #usb #usb #usb #stm32 #stm32 #stm32f4 #usb #discovery #stm32f3- Labels:
-
STM32F3 Series
-
STM32F4 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-09-12 06:48 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-09-12 11:16 PM
please check if you use the right interface aswell as the right pins
HAL_PCD_MspInit()
, but i would say: disable vbus sensing...check in your usbd_conf.c:USBD_StatusTypeDef USBD_LL_Init (USBD_HandleTypeDef *pdev)
{ /* Init USB_IP */ if (pdev->id == DEVICE_FS) { /* Link The driver to the stack */ hpcd_USB_OTG_FS.pData = pdev; pdev->pData = &hpcd_USB_OTG_FS; hpcd_USB_OTG_FS.Instance = USB_OTG_FS; hpcd_USB_OTG_FS.Init.dev_endpoints = 4; hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL; hpcd_USB_OTG_FS.Init.dma_enable = DISABLE; hpcd_USB_OTG_FS.Init.ep0_mps = DEP0CTL_MPS_64; hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED; hpcd_USB_OTG_FS.Init.Sof_enable = DISABLE; hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE;hpcd_USB_OTG_FS.Init.vbus_sensing_enable = DISABLE;
hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE; if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK) { while(1);//Error_Handler(); } HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80); HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 0, 0x40); HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 1, 0x80); } return USBD_OK;}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-09-13 07:08 AM
* I tried both with and without vbus sensing but it didn't change anything.
**I have checked theHAL_PCD_MspInit()
function and it's the right pins that are being configured (PA11 and PA12) in the right mode I think. Here is the function in usbd_conf.c file:/* MSP Init */void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle){ GPIO_InitTypeDef GPIO_InitStruct; if(pcdHandle->Instance==USB_OTG_FS) { /* USER CODE BEGIN USB_OTG_FS_MspInit 0 */ /* USER CODE END USB_OTG_FS_MspInit 0 */ /**USB_OTG_FS GPIO Configuration PA11 ------> USB_OTG_FS_DM PA12 ------> USB_OTG_FS_DP */GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Peripheral clock enable */ __HAL_RCC_USB_OTG_FS_CLK_ENABLE(); /* Peripheral interrupt init */ HAL_NVIC_SetPriority(OTG_FS_IRQn, 0, 0); HAL_NVIC_EnableIRQ(OTG_FS_IRQn); /* USER CODE BEGIN USB_OTG_FS_MspInit 1 */ /* USER CODE END USB_OTG_FS_MspInit 1 */ }}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-07 11:30 AM
I see your
HAL_PCD_MspInit() has the GPIO initialization for the USB pins. Mine has not. CubeMX generated. I cannot find this GPIO initialization happening anywhere else either.
STM32F042G6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-07 03:40 PM
Let me answer that myself. I found from STM32F072 example code for som eval board that GPIO initializing is optional.

- « Previous
-
- 1
- 2
- Next »