2024-02-10 2:50 AM - last edited on 2024-02-14 3:56 AM by Amel NASRI
I have a Nucleo-u5a5zj board and I want to connect a NewLand FM430 scanner that works as a virtual COM port. In the example, I only saw the USB CDC ACM device, but I only need the configuration for the host. Can you give me more explanation of what I should do? I tried using sources from other examples like USBX USB_HOST_CDC_ACM for STM32H7 and didn't get good results. Maybe someone can find me an example of how I can get a USB host in this configuration. Early thanks.
PS. I am trying to use AzureRTOS (ThreadX) and USBX
2024-02-10 4:54 AM
Maybe look at Tomasz USB host on Nucleo-u5a5 , how to do; and adapt for CDC .
https://github.com/tdjastrzebski/Nucleo-U5A5ZJ-USBX
2024-02-11 4:14 AM
What should I do to adapt for CDC?
2024-02-11 4:50 AM
Hi @GhostVVS,
Can you please enumerate your device with windows and share with us the descriptor of your device to see exactly what class and other informations to help you.
I recommande your thesycon tools or an usb analyzer.
https://www.thesycon.de/eng/usb_descriptordumper.shtml
Regards.
2024-02-11 5:57 AM
I don't use Windows.
2024-02-11 6:13 AM
> and didn't get good results
What you got ?
2024-02-11 7:18 AM
Do, do you have an USB trace that you can share with us or more information??
2024-02-11 10:25 AM
Nothing worked as I planned) I connected the scanner which is a VCP device and after trying to read the code it should return a ribbon with a link to the site (this is how it works when I connect it to a PC and open a connection in a terminal program). I thought that probably not everything is so simple and you can't just use the sources from the example for the host on the H7 series microcontroller