2015-04-06 2:56 AM
Hi all,
this sounds so simple but I did spend too many hours trying to just read data out from my HMC5883L 3-axis Magnetometer. I admitt I just switched from 8bit to the 32bit world, so bare with me... The ''new'' HAL drivers lack a bit of description and exsamples on the web so I ask you for help. Here the code; Cube MX generated on a 32F303 discovery board./* I2C2 init function */
void MX_I2C2_Init(void) {hi2c2.Instance = I2C2;
hi2c2.Init.Timing = 0x00201D2D; hi2c2.Init.OwnAddress1 = 0; hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED; hi2c2.Init.OwnAddress2 = 0; hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK; hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLED; hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLED; HAL_I2C_Init(&hi2c2);/**Configure Analogue filter
*/ HAL_I2CEx_AnalogFilter_Config(&hi2c2, I2C_ANALOGFILTER_DISABLED);}
&sharpdefine HMC5883L_MASTER_ADDR 0x13HAL_I2C_Mem_Read(&hi2c2,(uint16_t)HMC5883L_MASTER_ADDR,(uint16_t)X_MSB_Reg,I2C_MEMADD_SIZE_8BIT,(uint8_t*)readHMC5883LBuffer,6,100);
X_axis = make_word(readHMC5883LBuffer[0],readHMC5883LBuffer[1]);
Z_axis = make_word(readHMC5883LBuffer[2],readHMC5883LBuffer[3]); Y_axis = make_word(readHMC5883LBuffer[4],readHMC5883LBuffer[5]); The SCL pin goes low a few cycles and then time out gets called... Thanks for some suggestions! #stm32-hal-i2c2015-04-06 5:56 AM
heh. i was also playing around with stm32cube HAL over the weekend, with the mpu6050 instead.
a couple of notes: - i think the common address for the 5883 is 0x1E? you mentioned 0x13 in your code. - in any case, you might need to shift the device address left by 1 when calling the HAL_I2C_* routines (see below). - you can callHAL_I2C_IsDeviceReady()
to test if an i2c device is responding on the other side of the bus (just as a basic connectivity test)
while (HAL_I2C_IsDeviceReady(&hi2c2, (uint16_t) MPU6050_ADDRESS, 10, 100) != HAL_OK) {
... where the MPU6050 I2C address is 0x68
#define MPU6050_ADDRESS (0x68 << 1)
- probably minor, i also initialized two fields in the setup
hi2c2.Init.ClockSpeed = 400000;
hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_2;
2015-04-07 1:23 AM
thx noobee for your feedback! Yes silly me, 0x1E is the device address.
The Init.ClockSpeed and Init.DutyCycle is not member of my I2C_InitTypeDef. I guess my Init.Timing takes care of that. Anyway I do not get any data on SDA line. The I2C bursts out bundles of 100kHz (normal mode) puls-packages but no SDA Responses so far...