2015-10-29 5:58 AM
Hello all,
I have a strange question regarding speed od USB CDC and USB MSD driver for STM32F429.I implemented USB MSD + eMMC with FatFS support and I am getting 0.51 MB/s write and 0.69 MB/s read speed results with USB Flash Benchmark app (on Windows).Now I implemented USB CDC and I am generating 100MB of data and sending out to USB. Write speed (sending from FW to PC) is only 75kB/s .I expected CDC should be faster than result frm MSD + eMMC test. I do not know, what else to check or test to achieve higher speeds.I have USB FS type on the board. HS is not possible due to hardware design.What speed should I normally get from this setups?Thanks, Uros #stm32f429-usb-msd-cdc-speed2015-10-29 6:15 AM
Well the MSC can respond with at least 512 bytes per request, often significantly more. 600-700 KBps would be expected. The CDC likely sends a handful of bytes per packet, with more back-n-forth handshaking, probably not going to hit those kinds of numbers. Look at how you can fill every packet that crosses the wire.
2015-10-29 6:17 AM
I just benchmarked my STM32F407-based device. It's working at 48MHz, SDIO is at 24MHz, I'm using FatFS + SDIO (2GB SandDisk microSD) + USB FS Mass Storage.
read speed is ~800KB/s write speed is ~460KB/s The speeds are not very different from your case.2015-10-29 6:30 AM
I am generating dummy data, buffer size is 64 and I am sending this buffer to CDC.
uint32_t testSize = 100000000; //100MB
uint32_t dummyCounter = 0;
uint8_t APP_TX_DATA_SIZE = 64;
uint8_t buff_TX[APP_TX_DATA_SIZE];
for(uint8_t i = 0; i < APP_TX_DATA_SIZE; i++)
{
buff_TX[i] = i;
}
uint64_t StartTimeStamp = iMos_SysDateTime_Get_SysLiveTime( iMos_TimeUnit_ms );
while(dummyCounter < (testSize / APP_TX_DATA_SIZE))
{
usbStatus = CDC_Transmit_FS(buff_TX, sizeof(buff_TX));
dummyCounter++;
}
uint64_t StopTimeStamp = iMos_SysDateTime_Get_SysLiveTime( iMos_TimeUnit_ms );
StopTimeStamp returns me back current value in miliseconds since the Task is started.
With USB MSD speed, I am satisfied, but not with USB CDC.
The RCC settings I used I posted
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32%20F429%20USB%20MSD%20with%20eMMC%20%2b%20FatFS&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1
. On board I have 32kHz (on LSE) and 24MHz (on HSE) crystal. APB1 and APB2 peripheral clocks are 42 MHz2015-10-29 6:41 AM
Tune your parameters in usbd_conf.h (I presume you are using STM32_USB-Host-Device_Lib_V2.1.0.
Try to increase the APP_RX_DATA_SIZE, make it 10240 for example, and decrease the CDC_IN_FRAME_INTERVAL value, for example set it 0. Also, check out this .2015-10-29 6:43 AM
Thanks! I will try this settings and I'll post results as soon as I have them.
2015-10-29 6:59 AM
I have usbd_conf.h, usbd_cdc_if.h and usbd_cdc.h . I cannot findCDC_IN_FRAME_INTERVAL setting nowhere. I am using HAL drivers in the project.
The files are in attachment. APP_RX_DATA_SIZE I suspect isCDC_DATA_FS_IN_PACKET_SIZE in my headers. ________________ Attachments : usbd_cdc.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0wI&d=%2Fa%2F0X0000000bfu%2F5y7ex47SF.fQtq87gYog_TB9qNtZVMitNue3adnc1FQ&asPdf=falseusbd_cdc_if.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0s1&d=%2Fa%2F0X0000000bfs%2FnZH_wMu8G4Dnyb6CcJT3ErJPnvWMwYOJGkgT1YRMkfA&asPdf=falseusbd_conf.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0wM&d=%2Fa%2F0X0000000bft%2F_w7ZTo.cWpQGmPNdrvrNbj6EXBjlKgzK4Q8Nv3dcpT4&asPdf=false2015-11-04 2:20 AM
Update to the thread:
I learned that the speed of USB CDC is highly depending on what you are doing with data on the PC side. TeraTerm freezes, Terminal by Br@y hangs after receiving large amount of data,... so I made my own terminal app for Windows and I learned that displaying received data takes much longer as only storing received data in temporary file. Result: displaying of data in real time is slowing down the transfer speed.When I was displaying data in my terminal app, speed was only around 15kB/s, then I changed processing, so now, when I am expecting to get large volume of data, I store it to temporary file and then display this file when transmission is done. With this change, I was able to get USB CDC speed around 775 kB/s (+/- 5 kB/s).============================================Test 7 sending 10 MB of data (tested with own terminal app - saving to file)START: 6055 msEND: 18949 ms=============10 MB / 12849 ms = 778 kB/s============================================Test 8 sending 100 MB of data (tested with own terminal app - saving to file)START: 6055END: 134934=============100 MB / 128879 ms = 775 kB/s============================================