2024-11-21 02:04 AM - edited 2024-11-21 02:05 AM
Hello ST Community,
for the STM32H5, STM32U5 and STM32U0 series, it is already possible to use USBX without ThreadX using CubeMX. After my research, I have a few questions:
Thank you very much
Solved! Go to Solution.
2024-11-21 09:08 AM
Hi @Rookie38
For example, this stack is licensed under SLA0044 Rev5/February 2018
This class is supported in ST Library stack with no examples in device mode. If you could justify the necessity, in application level
Here is a project provided in host mode : TM32CubeF7/Projects/STM32F769I_EVAL/Applications/USB_Host/MTP_Standalone at master · STMicroelectronics/STM32CubeF7
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-21 09:08 AM
Hi @Rookie38
For example, this stack is licensed under SLA0044 Rev5/February 2018
This class is supported in ST Library stack with no examples in device mode. If you could justify the necessity, in application level
Here is a project provided in host mode : TM32CubeF7/Projects/STM32F769I_EVAL/Applications/USB_Host/MTP_Standalone at master · STMicroelectronics/STM32CubeF7
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-21 11:28 AM
>>Are there plans for ST's USB stack to receive safety certificates such as IEC 61508 SIL4, IEC 62304 Class C etc. similar to USBX?
If such thing have perceived value, perhaps there are commercial options?