2024-08-14 10:08 PM
Hi there, I'm currently trying to setup the STM32_Touchsensing library.
I have already downloaded the library from
ST(https://github.com/STMicroelectronics/STM32CubeWB/blob/master/README.md#how-to-use).
How do I enable this Touch sensing library now that I have downloaded it
Thanks!
2024-08-14 11:09 PM
Hello @Parry
So, the STM32_Touchsensingis a middleware that can be used with some STM32 MCUs. So, all you have is to open CubeMX, select an MCU or a board that you are going to use (as i can see is an STM32WB) and start your project. On the configuration panel of CubeMX m, go to middleware and enable the STM32_Touchsensing (you lay also have some settings to do for the middleware parameters).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.