2025-08-08 3:32 AM - last edited on 2025-10-16 2:10 AM by Saket_Om
Hello everyone,
I’m programming a B-U585I-IOT02A board. My goal is to capture audio through the integrated microphone at a sampling rate of 44 kHz and then analyze it using callbacks.
I’m using the example provided by ST Electronics, the BSP, from which I use the audio functions, specifically:
BSP_AUDIO_IN_Record(0, (uint8_t*) RecBuff, RECBUFF_SIZE*2);
First, I initialize the structure like this:
BSP_AUDIO_Init_t AudioInit;
/* Select device depending on the Instance */
AudioInit.Device = AUDIO_IN_DEVICE_DIGITAL_MIC1;
AudioInit.SampleRate = AUDIO_FREQUENCY_44K;
AudioInit.BitsPerSample = AUDIO_RESOLUTION_16B;
AudioInit.ChannelsNbr = 1; AudioInit.Volume = 50; /* Not used */
if (BSP_AUDIO_IN_Init(0, &AudioInit) != BSP_ERROR_NONE) {
Error_Handler();
}
The issue I’m facing is: when I use a RecBuff (of type uint16_t) with a length of 44100, I get a callback every 250 milliseconds instead of every second.
However, with a sampling rate of 11 kHz and a RecBuff length of 11000, I get exactly one callback per second, which is expected.
Why is this happening?
I absolutely need the 44 kHz sampling to work.
Please, I hope someone familiar with this ST Electronics example can help me understand this behavior. Thank you very much!
2025-10-27 2:25 AM
Hello @lucadelf ,
The buffer size needs to be adjusted because 44 kHz is 4 times faster than 11 kHz. To get an interrupt every 1 ms, you should multiply the RECBUFF_SIZE by 4 when using 11 kHz.
Br