Skip to main content
Associate II
December 20, 2025
Solved

rt-thread project

  • December 20, 2025
  • 3 replies
  • 943 views

I created project in stmcube32mx for h5 microcontroller and it works if I manually replace bl main to bl entry

in file startup_stm32h563zitx.s.

If this manual replacing is a bug or on purpose?

Jan

Best answer by KnarfB

This seems to be a very rt-thread specific topic and you might find specific help in their forum. 

hth

KnarfB

3 replies

KnarfB
Super User
December 21, 2025

Never heard of such a purpose. 

What does " it works" (or not) mean precisely? Linker errors? 

What version of STM32CubeMX and H5 firmware are you using?

Middlewares? 

Maybe you can post your .ioc file.

hth

KnarfB

 

Jan27Author
Associate II
December 23, 2025

Thank you for noticing my post.

After generating the project I noticed that in the file startup_stm32h563zitx.s (discovery board) still

there is bl main. I think it should be bl entry.

Program compiles in every situation but without changing to entry tasks don't run.

/* Call the application's entry point.*/

/* bl main */

bl entry

ST Employee
December 24, 2025

@Jan27  

Could you please provide the version of CubeMX and CubeIDE you are using?

I generated the project using your .ioc file with CubeMX version 6.16 and STM32CubeIDE version 1.19. I also tested it with bl main, and the execution runs without any issues.

Could you please specify the exact problem you encountered?

BR

Lobna

KnarfB
KnarfBBest answer
Super User
December 27, 2025

This seems to be a very rt-thread specific topic and you might find specific help in their forum. 

hth

KnarfB

Jan27Author
Associate II
December 28, 2025

Ok, it works for me now but I would expect that ST did something that it worked without manual adjusting

or clearly wrote what to do.

Jan

ST Employee
December 29, 2025

Dear @KnarfB @Jan27 

I will escalate this issue internally to enhance the ST documentation. Meanwhile, you may implement the recommended solution in the file Middlewares\Third_Party\RealThread_RTOS_RT-Thread\src\components.c when using the GCC compiler.
Specifically, at line 159:
/* Add -eentry to the arm-none-eabi-gcc linker arguments */

BR

Lobna

 
Jan27Author
Associate II
December 31, 2025

I see, thank you

Jan