2021-09-23 04:25 AM
Hello together,
after a lot of trouble getting the USB HS port working on the STM32H747 on the STM32H747I-DISCO Discovery kit I’m stuck again. I’m using STM Cube IDE 1.7 and the HAL USB CDC lib.
I was able to get USB CDC working on the M4 thanks to https://community.st.com/s/question/0D53W000002diUsSAI/stm32cubemx-h7x5h7x7-usb-cdc-bug
On the M7 core it kind of worked out of the box. But when I want to use it with the USB interal DMA enabled it didn’t work at all.
I already figured out I have to disable the D-cache and not use the DTCM SRAM for the buffer: https://community.st.com/s/article/how-to-enable-dma-in-usb-with-stm32h7-devices
I provided a minimal example of code which already results in failure:
...
MX_GPIO_Init();
MX_USB_DEVICE_Init();
HAL_Delay(1000);
uint8_t buffer1[2000], buffer2[2000];
CDC_Transmit_HS(buffer1, 1468);
HAL_Delay(50);
CDC_Transmit_HS(buffer2, 4);
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
When I use CDC_Transmit_HS() it works. I can send data from the provided buffer. I can also do this multiple times. And the DMA seems to work, as the execution time of CDC_Transmit_HS() is rather short and independent of the buffer length.
BUT: I can only send 1468 bytes of data. If I use a buffer length > 1468 bytes it doesn’t send anything.
If I send say CDC_Transmit_HS(buffer1, 1460) and than CDC_Transmit_HS(buffer1, 12) I get the first 1460 bytes transferred but the second call is not transmitted.
I also tried different memory addresses for the buffer pointer. E.g. 0x30020000 (SRAM2).
Always the same.
After the CDC_Transmit_HS() the CPU is normally executing code, just without any data being sent.
Any idea what I am doing wrong? With internal IP DMA disabled it works fine with large buffers and repeatably.
Thanks a lot
Solved! Go to Solution.
2021-10-13 01:34 AM
Hello @FTrie.1
Actually the following USB FIFO configuration is not correct when USB DMA is enabled.
/* USER CODE BEGIN TxRx_Configuration */
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x174);
/* USER CODE END TxRx_Configuration */
In fact, you should not allocate more than (4096 – 72 (for DMA descs)) bytes in total -> 0x3EE words
Please try to use the following config which should work for your use case.
/* USER CODE BEGIN TxRx_Configuration */
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x100);
/* USER CODE END TxRx_Configuration */
Please let me know if this solved your issue.
BeST Regards,
Walid
2021-10-08 06:34 AM
Hello @FTrie.1 ,
Your problem has been raised internally for verification. I will keep you updated.
Thanks for your contribution.
BeST Regards,
Walid
2021-10-08 07:52 AM
Hello @FTrie.1 ,
Potentially an USB FIFO configuration issue on the software that corrupt USB DMA descriptors.
Can you please provide the USB FIFO settings.
Thanks in advance.
BeST Regards,
Walid
2021-10-12 08:26 AM
Hello @FTrie.1
Are there any news concerning this issue from your side?
BeST Regards,
Walid
2021-10-12 11:08 AM
Hello @Walid ZRELLI ,
i haven't looked into it recently, as i changed my design and don't use the USB any longer. But it would still be interesting why it is not working using the HAL driver and dma enabled.
In 2 days i have access to the STM32H747I-DISCO Discovery kit again and will try again.
Regarding fifo settings, do you mean inside the function USBD_LL_Init(...) in usbd.conf.c? I haven't changed any of this:
USBD_StatusTypeDef USBD_LL_Init(USBD_HandleTypeDef *pdev)
{
/* Init USB Ip. */
if (pdev->id == DEVICE_HS) {
/* Link the driver to the stack. */
hpcd_USB_OTG_HS.pData = pdev;
pdev->pData = &hpcd_USB_OTG_HS;
hpcd_USB_OTG_HS.Instance = USB_OTG_HS;
hpcd_USB_OTG_HS.Init.dev_endpoints = 9;
hpcd_USB_OTG_HS.Init.speed = PCD_SPEED_HIGH;
hpcd_USB_OTG_HS.Init.dma_enable = ENABLE;
hpcd_USB_OTG_HS.Init.phy_itface = USB_OTG_ULPI_PHY;
hpcd_USB_OTG_HS.Init.Sof_enable = DISABLE;
hpcd_USB_OTG_HS.Init.low_power_enable = DISABLE;
hpcd_USB_OTG_HS.Init.lpm_enable = DISABLE;
hpcd_USB_OTG_HS.Init.vbus_sensing_enable = DISABLE;
hpcd_USB_OTG_HS.Init.use_dedicated_ep1 = DISABLE;
hpcd_USB_OTG_HS.Init.use_external_vbus = DISABLE;
if (HAL_PCD_Init(&hpcd_USB_OTG_HS) != HAL_OK)
{
Error_Handler( );
}
#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)
/* Register USB PCD CallBacks */
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_SOF_CB_ID, PCD_SOFCallback);
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_SETUPSTAGE_CB_ID, PCD_SetupStageCallback);
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_RESET_CB_ID, PCD_ResetCallback);
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_SUSPEND_CB_ID, PCD_SuspendCallback);
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_RESUME_CB_ID, PCD_ResumeCallback);
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_CONNECT_CB_ID, PCD_ConnectCallback);
HAL_PCD_RegisterCallback(&hpcd_USB_OTG_HS, HAL_PCD_DISCONNECT_CB_ID, PCD_DisconnectCallback);
HAL_PCD_RegisterDataOutStageCallback(&hpcd_USB_OTG_HS, PCD_DataOutStageCallback);
HAL_PCD_RegisterDataInStageCallback(&hpcd_USB_OTG_HS, PCD_DataInStageCallback);
HAL_PCD_RegisterIsoOutIncpltCallback(&hpcd_USB_OTG_HS, PCD_ISOOUTIncompleteCallback);
HAL_PCD_RegisterIsoInIncpltCallback(&hpcd_USB_OTG_HS, PCD_ISOINIncompleteCallback);
#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */
/* USER CODE BEGIN TxRx_Configuration */
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x174);
/* USER CODE END TxRx_Configuration */
}
return USBD_OK;
}
2021-10-13 01:34 AM
Hello @FTrie.1
Actually the following USB FIFO configuration is not correct when USB DMA is enabled.
/* USER CODE BEGIN TxRx_Configuration */
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x174);
/* USER CODE END TxRx_Configuration */
In fact, you should not allocate more than (4096 – 72 (for DMA descs)) bytes in total -> 0x3EE words
Please try to use the following config which should work for your use case.
/* USER CODE BEGIN TxRx_Configuration */
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x100);
/* USER CODE END TxRx_Configuration */
Please let me know if this solved your issue.
BeST Regards,
Walid
2021-10-13 11:42 PM
Hello @Walid ZRELLI ,
i just tried it with the new USB FIFO settings and it works. Thanks a lot!
Hopefully this will help others with the same problem 🙂
2021-10-14 12:32 AM
Hello @FTrie.1
Glad to help you 😊
Please click on Select as Best if my post fully answered your question. This will help other customers with the same issue to find the solution faster!
BeST Regards,
Walid