Problem with SMBus communication
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-07-04 3:04 AM
Hi, I've been trying for a few days to communicate with a device by SMBus.
The device is an Microchip USB2422 and for test I use board DISC1 with STM32F429 on i2c3 port.
The problem is that when I try to communicate with it to oscilloscope I see only a single signal with 10ms duration on both SCL and SDA.
Then I tried with another device (INA219) and that works on I2C and SMBus.
With I2C I can work with it without any problem, but with SMBus (with same connection) I've the same problem of USB2422.
Is there something I'm missing?
Thanks.
Labels:
- Labels:
-
I2C
-
STM32F4 Series
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0