2019-10-12 9:02 PM
Hi.
I'm working on a STM32F4-Discovery board, and I'm having trouble linking the PDM2PCM Library into my project.
I have run the example project located in the STM32F4-Discovery folder called "Audio_playback_and_record" and it works fine.
I have copied the settings from this project into my new CUBE project, but when I run the compiler I get the following message
arm-none-eabi/bin/ld.exe: cannot find -l:libPDMFilter_CM4_GCC_wc32.a.
below is an image of my settings, can anyone help me solve this issue?
2020-12-10 9:09 AM
I've been fighting with the SAI sub-system and the PDM2PCM library as well. I can offer some insights on the PDM2PCM library, but I am still having high frequency noise issues.
As I understand it, it is expecting data to be in a byte packet format. This means on a one microphone system you have something like this:
| 8-bits of PDM data | 8-bits of PDM data | ..... | 8-bits of PDM data |
When you call PDM_Filter, you pass in this buffer of data as well as the PCM output buffer. You need to set your decimation factor and your output_samples_number:
PDM1_filter_config.output_samples_number = 1024;
In my case I have 1.536 MHz PDM clock and am decimating by 64. I am using a 8192 byte buffer to hold the PCM data (8192 * 8 bits = 65536 PDM bits)
65536 PDM bits / 64 (decimation) = 1024 PCM samples (16-bit samples).
In my case I'm using two microphones. So the PDM data is packed liks this:
| 8-bits left mic | 8-bits right mic | | 8-bits left mic | 8-bits right mic | ....
Then when you call PDM_Filter, you get:
|16-bit PCM left mic | 16-bit PCM right mic | .....
My problem is I get high frequency noise. It seems like the filter isn't actually filtering. It seems more like it is decimating in time without the low pass filter.
2020-12-10 9:13 AM
The post is from over a year ago, poster has likely moved on..