cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO-LRWAN2

Grey
Associate

I have the P-NUCLEO-LRWAN2 package. The Gateway (NUCLEO-F746ZG with the RisingHF ARDUINO® expansion board (LRWAN_GS_HF1) has a firmware VERSION: 2.1.7, Nov 6 2018. I was wondering if there is an update to the firmware and what the current version of the Semtech packet forwarder is? Tgh problem I am having is the current version does not publish the stats as example {"stat":{"time":"2014-01-12 08:59:28 GMT","lati":46.24000, "long":3.25230, "alti":145,"rxnb":2, "rxok":2,"rxfw":2, "ackr":100.0,"dwnb":2, "txnb":2}} copied from packet_forwarder/PROTOCOL.TXT at master · Lora-net/packet_forwarder (github.com). I am trting to connect to a ChirpStack server with AU915 reginal settings. 

Regardless of whether there is an update or not can I please get a copy the current bin file. 

1 REPLY 1
Rihen
Associate

I would need this too... 
I thought this was an opened developement kit i'm disappointed, and the support is not granted.