cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleof446re DAC

harry123
Senior II

Hi 

  • I am trying to generate a Dc volatge ramp signal 0 to 1v and 1v to 0 
  • I want to stop the signal on pressing the user button pc13.
  • I am able stop the dac but the output on pin PA4 with respect to gnd  is 0.02V 
#include "stm32f4xx_hal.h"

// Define DAC handle and resolution
DAC_HandleTypeDef hdac;
#define DAC_RESOLUTION 1241   
// Button press flag
volatile uint8_t button_pressed = 0;

// Function to initialize DAC
void DAC_Init(void)
{
    __HAL_RCC_DAC_CLK_ENABLE();  // Enable DAC clock

    hdac.Instance = DAC;
    HAL_DAC_Init(&hdac);  // Initialize DAC

    DAC_ChannelConfTypeDef sConfig = {0};
    sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
    sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;  // Disable output buffer
    HAL_DAC_ConfigChannel(&hdac, &sConfig, DAC_CHANNEL_1);
    HAL_DAC_Start(&hdac, DAC_CHANNEL_1);  // Start DAC
}

// Function to initialize button (PC13)
void Button_Init(void)
{
    GPIO_InitTypeDef GPIO_InitStruct = {0};
    __HAL_RCC_GPIOC_CLK_ENABLE();

    GPIO_InitStruct.Pin = GPIO_PIN_13;
    GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;  // Falling edge trigger (button press)
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

    // Enable EXTI interrupt for line 13 (PC13)
    HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
}

// Interrupt handler for button press (PC13)
void EXTI15_10_IRQHandler(void)
{
    static uint32_t last_interrupt_time = 0;
    uint32_t interrupt_time = HAL_GetTick();

    if (__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_13) != RESET)
    {
        // Clear the interrupt flag
        __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_13);

        // Simple debounce check: ignore if the interrupt happens too quickly after the last one
        if (interrupt_time - last_interrupt_time > 50)  // 50 ms debounce
        {
            last_interrupt_time = interrupt_time;

            // Set flag to indicate button press
            button_pressed = 1;
        }
    }
}

// Ramp DAC function (0 to 1V and back)
void Ramp_DAC(void)
{
    uint32_t dacValue;
    int32_t direction = 1; // Ramp direction: 1 = up, -1 = down

    while (1)
    {
        // Polling button press status in main loop
        if (button_pressed)
        {
            // Set DAC to 0V (explicitly force DAC to 0)
            HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0);
            
            // Stop the DAC output to force it to 0V
            HAL_DAC_Stop(&hdac, DAC_CHANNEL_1);
            break;  // Stop the ramp
        }

        // Ramp the DAC value
        if (direction == 1)
        {
            for (dacValue = 0; dacValue < DAC_RESOLUTION; dacValue++)
            {
                HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, dacValue);
                HAL_Delay(1);  // Adjust ramp speed
            }
            direction = -1;  // Change direction to ramp down
        }
        else
        {
            for (dacValue = DAC_RESOLUTION; dacValue > 0; dacValue--)
            {
                HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, dacValue);
                HAL_Delay(1);  // Adjust ramp speed
            }
            direction = 1;  // Change direction to ramp up
        }
    }
}

int main(void)
{
    HAL_Init();
    DAC_Init();
    Button_Init();
    Ramp_DAC();

    while (1)
    {
        
    }
}​
  • whereas i can measure 0.001v smallest volatge 
  • I want the value 0 or close to zero on pressing user button I have attached the code below

Thank you.

1 REPLY 1
mƎALLEm
ST Employee

Hello,

What do you mean by "the value 0 or close to zero"? 

Already answered the question here.

mALLEm_2-1742374213859.png

As you've disabled the DAC output buffer:

 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;  // Disable output buffer

The value of DAC OUT min is given in the datasheet: 0.5mV as Typical

With measurement errors + PCB (NUCLEO is not optimized for analog) I don't think you can go lower than that.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.