2023-10-25 3:00 AM
Hello ,
Import example code from package en.stm32cubeh5-v1-1-0\STM32Cube_FW_H5_V1.1.0\Projects\NUCLEO-H503RB\Applications\USBX\Ux_Device_CDC_ACM
and Run the example using STMcubemx IDE
Gives hard fault error when call function
ux_dcd_stm32_initialize((ULONG)USB_DRD_FS, (ULONG)&hpcd_USB_DRD_FS);
2023-11-23 5:48 AM - edited 2023-11-29 7:27 AM
Hello @pooja ,
Sorry for the late reply. Is the Ux_Device_CDC_ACM still not working?
Could you please add these code lines into the .ld file as detailed in readme:
._threadx_heap :
{
. = ALIGN(8);
__RAM_segment_used_end__ = .;
. = . + 64K;
. = ALIGN(8);
} >RAM_D1 AT> RAM_D1
Also, try to use the last STM32Cube_FW_H5_V1.1.1 package.
Please let me know if the issue is solved or not.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.