2024-10-02 7:38 PM
Hardware:
NUCLEO-F446RE, X-NUCLEO-CCA01M1, X-NUCLEO-CCA02M2
Software:
SMARTMIC1 V2.4.0 & V2.3.0
I am attempting to run the SMARTMIC1 program on the hardware list above but instead of using the microphones on the STEVAL-MIC001V1, I want to use the CCA02M2 onboard MP34DT06J microphones.
In an attempt to achieve this on CCA02M2 I changed the position of J2 to position 1-2, removed J3, and installed the solder bridge on SB9.
While Audacity will start recording, 0 microphone volume is recorded.
I am now looking into the cca02m2_conf.h file and change the AUDIO_IN_CHANNELS from 4 to 2.
In Audacity, channel 2 is 100% volume, and channel 1 is 0% volume.
Is there any way to achieve what I am trying to do?
2024-10-15 7:26 AM
Hello @OceanPlumber
The SMARTMIC1 demo is meant to work with 4 microphones only. Updating the cca02m2_conf.h
file is not sufficient.
The demo uses a custom USB class that allows both USB audio communication and serial communication so that the firmware can be controlled by the GUI distributed in the package. It is a complex setup, designed to showcase the Acoustic libraries at their maximum capacity.
If you'd like to focus your attention on easier examples, I suggest you look into X-CUBE-MEMSMIC1, where you can find a specific example for any of the audio in related Acoustic library. Natively, it supports NUCLEO-F401RE, but porting it to NUCLEO-F446RE is straightforward (both Nucleo boards use the same Cortex).
Best regards,
Simone