2020-03-16 4:33 AM
Hello,
I have a problem with LWIP. LWIP doesn’t property work on Nucleo-144 STM32F746 with default settings. After three ping telegrams LWIP doesn’t work anymore and FreeRTOS tasks are blocked.
DHCP is activated and I get IP dynamically from DHCP-Server.
I use STM32CubeIDE 1.3.0. All configuration I have done with STM32CubeIDE and use a default settings of STM32Cube.
Follow steps I have done:
Task definition:
/* Definitions for defaultTask */
osThreadId_t defaultTaskHandle;
const osThreadAttr_t defaultTask_attributes = {
.name = "defaultTask",
.priority = (osPriority_t) osPriorityNormal,
.stack_size = 256 * 4
};
/* Definitions for AliveTask */
osThreadId_t AliveTaskHandle;
const osThreadAttr_t AliveTask_attributes = {
.name = "AliveTask",
.priority = (osPriority_t) osPriorityLow,
.stack_size = 128 * 4
};
Tasks:
/* USER CODE BEGIN Header_StartDefaultTask */
/**
* @brief Function implementing the defaultTask thread.
* @param argument: Not used
* @retval None
*/
/* USER CODE END Header_StartDefaultTask */
void StartDefaultTask(void *argument)
{
/* init code for LWIP */
MX_LWIP_Init();
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
HAL_GPIO_TogglePin(LD1_Green_GPIO_Port, LD1_Green_Pin);
osDelay(1000);
}
/* USER CODE END 5 */
}
/* USER CODE BEGIN Header_aliveTask */
/**
* @brief Function implementing the AliveTask thread.
* @param argument: Not used
* @retval None
*/
/* USER CODE END Header_aliveTask */
void aliveTask(void *argument)
{
/* USER CODE BEGIN aliveTask */
/* Infinite loop */
for(;;)
{
HAL_GPIO_TogglePin(LD2_Blue_GPIO_Port,LD2_Blue_Pin);
osDelay(500);
}
/* USER CODE END aliveTask */
}
What is wrong in default settings of STM32Cube?
Many thanks in advance.
2020-03-19 2:24 AM
I found the workaround. Instead CMSIS_V2, I chose the interface CMSIS_V1 for FreeRTOS. It works.
Can anyone explain the difference between CMSIS_V1 and CMSIS_V2?
Regards.
2020-03-19 4:24 PM
> Can anyone explain the difference between CMSIS_V1 and CMSIS_V2?
Apart form some different functionality and naming, which is documented and the official documentation is freely available online, another difference seems to be in the amount of bugs...
2020-03-20 2:17 AM
>>another difference seems to be in the amount of bugs...
It seems that V2 has more bugs than V1.;)
2020-03-20 4:15 AM
Hi Piranha,
I have tried to find why this configuration doesn’t work with V2.
It seems to be the old bug that you reported here:
https://community.st.com/s/question/0D50X0000BOtUflSQF/bug-stm32-lwip-ethernet-driver-rx-deadlock
void ethernetif_input(void const * argument)
{
struct pbuf *p;
struct netif *netif = (struct netif *) argument;
for( ;; )
{
if (osSemaphoreWait(s_xSemaphore, TIME_WAITING_FOR_INPUT) == osOK)
{
do
{
LOCK_TCPIP_CORE();
p = low_level_input( netif );
if (p != NULL)
{
if (netif->input( p, netif) != ERR_OK )
{
pbuf_free(p);
}
}
UNLOCK_TCPIP_CORE();
} while(p!=NULL);
}
}
The function low_level_input(...) returns NULL value, because the function HAL_ETH_GetReceivedFrame_IT(...) returns a value HAL_ERROR.
The ETH_DMARXDESC_OWN flag is set in heth->RxDesc->Status in HAL_ETH_GetReceivedFrame_IT(...) and a condition of while loop is false. The while loop isn't executed and the fuction returns HAL_ERROR.
HAL_StatusTypeDef HAL_ETH_GetReceivedFrame_IT(ETH_HandleTypeDef *heth)
{
uint32_t descriptorscancounter = 0;
/* Process Locked */
__HAL_LOCK(heth);
/* Set ETH HAL State to BUSY */
heth->State = HAL_ETH_STATE_BUSY;
/* Scan descriptors owned by CPU */
while (((heth->RxDesc->Status & ETH_DMARXDESC_OWN) == (uint32_t)RESET) && (descriptorscancounter < ETH_RXBUFNB))
{
//Skip...
}
/* Set HAL State to Ready */
heth->State = HAL_ETH_STATE_READY;
/* Process Unlocked */
__HAL_UNLOCK(heth);
/* Return function status */
return HAL_ERROR;
}
After a call of function osSemaphoreWait(...) the task is waiting for a semaphore and I have a deadlock.
Regards