cancel
Showing results for 
Search instead for 
Did you mean: 

Missing define for SPI6I2S on STM32H7

S58D4J
Associate

Some STM32H7 MCUs have I2S capability on SPI6, but the HAL does not define "SPI_SPI6I2S_SUPPORT" for all of them. The ones with the missing define gets the prescaler computed wrong if the clock for SPI123 and SPI6 is different.

 

Has HAL support:

H7B3
H7B0
H7A3

 

Has capability but missing HAL support:
H735
H733
H730
H725
H723

 

Manually adding the define fixes the issue, the prescaler is calculated correctly and the expected clock frequency is sent to the I2S pins.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @S58D4J ,

The issue is fixed in STM32CubeH7 1.11.2 version and in GitHUB.

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KDJEM.1
ST Employee

Hello @S58D4J and welcome to the Community :),

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 170995 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hi @S58D4J ,

The issue is fixed in STM32CubeH7 1.11.2 version and in GitHUB.

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.