Memory is corrupted from hUsbDeviceHS.ep_out[1].rem_length (0x2400162c) onwards.
- 7 replies
- 5685 views
Hello,
We are using the USB HAL library on our custom board with an STM32H753VIT6. We have an external PHY chip (USB3300) and USB_OTG_HS. At the moment, we are using the USB to receive custom protobuf packets with a bandwidth at around 480 kbps. We have also written some additional overhead for our custom packets.
Everything works mostly fine. However, after a second of running, some of our variables get corrupted. By looking at the build-analyzer in CubeIDE, I found that the RAM, namely the .bss section, was being set to garbage from 0x2400162c onwards. This was hUsbDeviceHS.ep_out[1].rem_length. I am not sure whether this variable is relevant to the problem or it is just a coincidence.
I know that this could be from our own code somewhere that has a memory-leak, but I am wondering if this has been found before. I tried searching online but found nothing. Otherwise, are there any tips specific to STM32 to tracking down the cause?
Thanks,