cancel
Showing results for 
Search instead for 
Did you mean: 

- Main Config: These peripherals still have some not configured or wrong parameter values: [CORTEX M7] getting error

MDeva.1
Associate II

Hello ,

I am working on NUCLEO-H745ziq board. I am trying the example AZURE RTOS of Ux_CDC_device , the example provide in cubemx accordingly I setup the things in cubemx but when I try to generate the code it shows warning and the when I run the programmed hard fault error is come. I follow the example of NUCLEO-H723ZG. all the setup same as I done why Iget these error ? can you please help me

0693W00000QKISWQA5.png

1 ACCEPTED SOLUTION

Accepted Solutions
sgiraz
Associate

You are probably missing a configuration for some parameters (i.e. if you configure MPU regions, you need to configure all of them, not just some of them).

View solution in original post

1 REPLY 1
sgiraz
Associate

You are probably missing a configuration for some parameters (i.e. if you configure MPU regions, you need to configure all of them, not just some of them).