Low power mode with ThreadX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-10 3:17 AM - edited ‎2024-10-10 3:43 AM
Hello all,
I am testing low power mode 2 using ThreadX but having a bit of a problem when waking up. I have generated a simple test, there is one task running blinking a led every second for 10 secs and then sending the MCU to low power mode 2, until this point all works okay.
I have got a button that will wake up the MCU by an interrupt when it is pressed and the unit should go and start blinking the LED every 1 sec for another 10 secs.
The MCU comes out of mode 2 when the the button is pressed but I am having a problem with the clock configuration when waking up, the led flashes at around 6 secs after waking up instead of every 1 sec.
Main routine:
VOID LED1_thread_entry(ULONG initial_input)
{
uint8_t counter = 0;
while(1)
{
HAL_GPIO_TogglePin(LED1_GPIO_Port, LED1_Pin);
tx_thread_sleep(1000);
counter++;
if(counter == 10)
{
counter = 0;
Enter_LowPower_Mode();
}
}
}
This is my routine that put the MCU into low power mode 2:
void Enter_LowPower_Mode(void)
{
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
}
This is the routine exiting the lo power mode2:
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
if(GPIO_Pin == Button_Pin)
{
Exit_LowPower_Mode();
}
}
void Exit_LowPower_Mode(void)
{
SystemClock_Config();
}
The clock configuration that I am using is:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 13;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
RCC_OscInitStruct.PLL.PLLFRACN = 4096;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
Any idea what the problem could be?
Thank you
- Labels:
-
STM32U5 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-10 6:58 AM - edited ‎2024-10-10 6:59 AM
Hello @jampino,
This is relatively known, as in some of our examples we already handle this by re-enabling the PLL and setting the correct clock source after waking up from low-power mode.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-10 7:04 AM
Hi @Sarra.S,
Is this what you are referring to: https://github.com/STMicroelectronics/STM32CubeU5/blob/main/Projects/NUCLEO-U575ZI-Q/Applications/ThreadX/Tx_LowPower/Src/app_threadx.c#L118
if not, could you point me to one of your examples please.
Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-10 7:15 AM
Yes!
Exactly here, restoring the initial SystemClock configuration after exiting a low-power mode:
void Exit_LowPower_Mode(void)
{
/* Enable AHB APB Peripheral Clock */
__HAL_RCC_AHB1_CLK_ENABLE();
__HAL_RCC_AHB2_1_CLK_ENABLE();
__HAL_RCC_AHB2_2_CLK_ENABLE();
__HAL_RCC_APB1_CLK_ENABLE();
__HAL_RCC_APB2_CLK_ENABLE();
/* Reconfigure the system clock*/
SystemClock_Restore();
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-10 7:32 AM
Thanks, tried before but still having the same results