2020-09-15 02:06 AM
2020-09-18 02:18 AM
Hi AJean.1,
In fact these files are part of ST deliveries for the flasher support, then these files get integrated within the EWARM workbench IDE, so I believe you can find more about the License limitation via this link: www.st.com/SLA0044
I advise you to download the latest version of EWARM (IAR) IDE in order to have access for the latest supported stm32 products. And you will find the .ddf files under a similar path in your C: directory: Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\ST
-Imen
2020-09-15 05:35 AM
Hi AJean.1,
To answer your question, no we don't have an equivalent to SVD files for memory description of STM32 SOCs. To explain more, SVD files are a way to translate the contents on the manual reference for different IPs for a given stm32 product. This Includes the different registers and fields etc...
Do you think you can provide an example of the result you wish to obtain, maybe I can guide you more then?
-Imen
2020-09-15 12:11 PM
Hello @Imen Ezzine ,
Thank you for your answer. The idea is to generate linker scripts like here automatically for any STM32 device.
Looking projects like this, it seems I might be able to steal data from CubeMX but having some official download link from ST with a fixed syntax might be better.
Alexis.
2020-09-17 04:42 AM
Hi AJean.1,
Sorry for late reply!
Now that your request seems more clear and looking on the example you gave me, I can think may be some files from the IDE EWARM (IAR) can help you. In fact from your example you need the Flash and RAM division predefined for different stm32 products right?
I believe it will be up to you to define a script to extract the infos you need which don't seem like a complicated task!
Let me know if this solve your problem?
Imlen
2020-09-17 12:42 PM
Hi @Imen Ezzine ,
.ddf files looks better to me, for two reason, first they seems easier to parse and second if they are form ST and I'm allowed to redistribute them in an open source project that would be awesome.
The only limitation I see here is that I might have to do some guess to find which RAM is CCM RAM, but that should be ok.
Where can I get ddf files?
Regards,
Alexis.
2020-09-18 02:18 AM
Hi AJean.1,
In fact these files are part of ST deliveries for the flasher support, then these files get integrated within the EWARM workbench IDE, so I believe you can find more about the License limitation via this link: www.st.com/SLA0044
I advise you to download the latest version of EWARM (IAR) IDE in order to have access for the latest supported stm32 products. And you will find the .ddf files under a similar path in your C: directory: Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\ST
-Imen