cancel
Showing results for 
Search instead for 
Did you mean: 

Is it needed for host pc to use static ip when working with LwIP ethernet?

Lpadd.1
Associate

Is it needed for host pc to use static ip when working with LwIP ethernet?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

LwIP can use DHCP, provided you have a DHCP server somewhere.

Static IP can be easier to set up.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Super User

LwIP can use DHCP, provided you have a DHCP server somewhere.

Static IP can be easier to set up.

If you feel a post has answered your question, please click "Accept as Solution".
Lpadd.1
Associate

@TDK​ If I use a static ip on my host pc and a static ip on the stm32, do they have to be set differently or do they need to be the same?

TDK
Super User

They should be different. Two devices on a network should never have the same IP.

If you feel a post has answered your question, please click "Accept as Solution".