2021-11-26 06:36 AM
It 's seem to me there is an error page 2651 of RM0468, STMH730 reference manual.
the figure 782 has a Current limited power switch in the design, but if un understand corretly, is only need in OTG host or dual role device.
Am I correct ? there is no need of current limited power switch on Vbus in peripheral only ?
Solved! Go to Solution.
2021-11-26 06:40 AM
Welcome, @Tbill.1, to the community!
Yes, you are right. It is also mentioned in the caption:
1. (Instead) Use a regulator to build a bus-powered device.
Regards
/Peter
2021-11-26 06:40 AM
Welcome, @Tbill.1, to the community!
Yes, you are right. It is also mentioned in the caption:
1. (Instead) Use a regulator to build a bus-powered device.
Regards
/Peter