cancel
Showing results for 
Search instead for 
Did you mean: 

IP stack support for H5 series

MSGokul
Associate

Why doesn't ST provide LWIP support for H5 series. Otherwise is there any option to add any other IP stack directly configurable from StmCubeIDE?

1 REPLY 1
STea
ST Employee

Hello @MSGokul ,

The AZURE Netxduo networking stack is officially supported for the H5 series you can find examples of its implementation in our cube firmware under your specific board folder application here is a link to the example of the STM32H573 

LWIP is supported as it is ported in STMicroelectronics/stm32h5-classic-coremw-apps: Provide a set of applications for STM32H5xx series based on the STM32 Classic Core Middleware libraries. (github.com)

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.