2018-10-04 7:07 PM
Hi all, I've tried to integrate Nucleo-F411RE with X_Nucleo-IDW01ME by using C:\Users\WIFI_IDW01M1\en.x-cube-wifi1_firmware\STM32CubeExpansion_WIFI1_V3.1.1\Projects\Multi\Applications\HTTP_Request\Binary\SPWF01\STM32F401RE-Nucleo .bin file and using the serial port to read if the connection is successful. Unfortunately, it shows me the picture below, i reckon it doesn't work properly as desired. I have tried once where it successfully connected and giving out feedback such as >>connected.......
But once I tried again it doesn't response anything.