2023-04-04 9:35 PM
2023-04-04 9:40 PM
Push in via an External Loader, pull via Ethernet, or USB Flash Drive (MSC Host)
2023-04-04 11:07 PM
Do you have a sample?
2023-04-05 2:00 AM
Not something I'm working on. Perhaps look if there is an example MSC Device using the eMMC directly?
2023-04-06 7:27 AM
Hello @wsuwa.1,
For audio file, you can get inspired with the example provided for STM32H747I-DISCO as referenced here.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.